Dear NXP Community,
I have imx7dsabresd board and was able to build yocto from fsl-community-bsp and loaded fine (kernel: linux-imx_4.1.15)
Now, I want to modify the kernel config and before doing that just want to understand how the two defconfig files are used by yocto to generate the ".config" file.
meta-freescale/recipes-kernel/linux/linux-imx-4.1.15/imx/defconfig
kernel source tree: arch/arm/configs/imx_v7_defconfig
Could you point me the recipe(s) or documentation that I can go throught?
Thanks,
Carlos
Hello,
Please use the following regarding Building Linux Kernel
Also, please look at the following :
Kernel config file used by Yocto
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------