imx6ull yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ull yocto

1,064 次查看
2548903578
Contributor III

After I compile bitbake core-image-minimal -c populate_sdk, the following error is displayed:

 

ERROR: nativesdk-util-linux-2.34-r0 do_compile: oe_runmake failed
ERROR: nativesdk-util-linux-2.34-r0 do_compile: Execution of '/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/temp/run.do_compile.12989' failed with exit code 1:
make all-recursive
make[1]: Entering directory '/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/build'
Making all in po
make[2]: Entering directory '/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/build/po'
make[2]: Nothing to be done for 'all'.
make[2]: Leaving directory '/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/build/po'
make[2]: Entering directory '/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/build'
./x86_64-pokysdk-linux-libtool --tag=CC --mode=link x86_64-pokysdk-linux-gcc --sysroot=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/recipe-sysroot -fsigned-char -fno-common -Wall -Werror=sequence-point -Wextra -Wmissing-declarations -Wmissing-parameter-type -Wmissing-prototypes -Wno-missing-field-initializers -Wredundant-decls -Wsign-compare -Wtype-limits -Wuninitialized -Wunused-but-set-parameter -Wunused-but-set-variable -Wunused-parameter -Wunused-result -Wunused-variable -Wnested-externs -Wpointer-arith -Wstrict-prototypes -Wimplicit-function-declaration -Wdiscarded-qualifiers -I./libblkid/src -I./libmount/src -I./libsmartcols/src -O2 -pipe -fmacro-prefix-map=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0=/usr/src/debug/nativesdk-util-linux/2.34-r0 -fdebug-prefix-map=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0=/usr/src/debug/nativesdk-util-linux/2.34-r0 -fdebug-prefix-map=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/recipe-sysroot= -fdebug-prefix-map=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/recipe-sysroot-native= -Wl,-O1 -o lsblk misc-utils/lsblk-lsblk.o misc-utils/lsblk-lsblk-mnt.o misc-utils/lsblk-lsblk-properties.o misc-utils/lsblk-lsblk-devtree.o libblkid.la libmount.la libcommon.la libsmartcols.la
./x86_64-pokysdk-linux-libtool --tag=CC --mode=link x86_64-pokysdk-linux-gcc --sysroot=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/recipe-sysroot -fsigned-char -fno-common -Wall -Werror=sequence-point -Wextra -Wmissing-declarations -Wmissing-parameter-type -Wmissing-prototypes -Wno-missing-field-initializers -Wredundant-decls -Wsign-compare -Wtype-limits -Wuninitialized -Wunused-but-set-parameter -Wunused-but-set-variable -Wunused-parameter -Wunused-result -Wunused-variable -Wnested-externs -Wpointer-arith -Wstrict-prototypes -Wimplicit-function-declaration -Wdiscarded-qualifiers -I./libmount/src -I./libsmartcols/src -I./libblkid/src -O2 -pipe -fmacro-prefix-map=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0=/usr/src/debug/nativesdk-util-linux/2.34-r0 -fdebug-prefix-map=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0=/usr/src/debug/nativesdk-util-linux/2.34-r0 -fdebug-prefix-map=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/recipe-sysroot= -fdebug-prefix-map=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/recipe-sysroot-native= -Wl,-O1 -o findmnt misc-utils/findmnt-findmnt.o misc-utils/findmnt-findmnt-verify.o libmount.la libcommon.la libsmartcols.la libblkid.la
./x86_64-pokysdk-linux-libtool --tag=CC --mode=link x86_64-pokysdk-linux-gcc --sysroot=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/recipe-sysroot -fsigned-char -fno-common -Wall -Werror=sequence-point -Wextra -Wmissing-declarations -Wmissing-parameter-type -Wmissing-prototypes -Wno-missing-field-initializers -Wredundant-decls -Wsign-compare -Wtype-limits -Wuninitialized -Wunused-but-set-parameter -Wunused-but-set-variable -Wunused-parameter -Wunused-result -Wunused-variable -Wnested-externs -Wpointer-arith -Wstrict-prototypes -Wimplicit-function-declaration -Wdiscarded-qualifiers -I./libmount/src -O2 -pipe -fmacro-prefix-map=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0=/usr/src/debug/nativesdk-util-linux/2.34-r0 -fdebug-prefix-map=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0=/usr/src/debug/nativesdk-util-linux/2.34-r0 -fdebug-prefix-map=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/recipe-sysroot= -fdebug-prefix-map=/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/recipe-sysroot-native= -Wl,-O1 -o fstrim sys-utils/fstrim-fstrim.o libcommon.la libmount.la
x86_64-pokysdk-linux-libtool: error: 'libcommon.la' is not a valid libtool archive
make[2]: *** [Makefile:6854: fstrim] Error 1
make[2]: *** Waiting for unfinished jobs....
x86_64-pokysdk-linux-libtool: error: 'libblkid.la' is not a valid libtool archive
make[2]: *** [Makefile:6993: lsblk] Error 1
x86_64-pokysdk-linux-libtool: error: 'libmount.la' is not a valid libtool archive
make[2]: *** [Makefile:6813: findmnt] Error 1
make[2]: Leaving directory '/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/build'
make[1]: *** [Makefile:13027: all-recursive] Error 1
make[1]: Leaving directory '/home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/build'
make: *** [Makefile:5620: all] Error 2
WARNING: exit code 1 from a shell command.

ERROR: Logfile of failure stored in: /home/zxs/imx6/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-util-linux/2.34-r0/temp/log.do_compile.12989

How should I solve it, hope to get a reply!

0 项奖励
回复
1 回复

1,054 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You must forgot something to install in your host, or do you try to compile it with out delete everything and burn again. 

https://docs.yoctoproject.org/dev-manual/start.html

 

Regards

0 项奖励
回复