imx6ull write/read operations to spi nor flash failing in u-boot console

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6ull write/read operations to spi nor flash failing in u-boot console

跳至解决方案
4,630 次查看
carbar
Contributor I

Hello, 

I'm having problems accessing spi nor flash using u-boot console. Write/read operations are failing unless data size is small.

=> sf probe
SF: Detected W25Q16JV with page size 256 Bytes, erase size 64 KiB, total 2 MiB
=> sf erase 0 0x200000
SF: 2097152 bytes @ 0x0 Erased: OK
=> mw.b 0x00900000 0x0 0x20000
=> mtest 0x00900000 0x0090ffff 0x12345678 0x1
Testing 00900000 ... 0090ffff:
Pattern 12345678 Writing... Reading...Tested 1 iteration(s) with 0 errors.
=>

Write operation:

=> sf write 0x00900000 0x0 0x1000
device 0 offset 0x0, size 0x1000
SF: 4096 bytes @ 0x0 Written: OK
=>

2020-03-04-2-imx6ullcom-4_spi_nor_signals_write.jpg

I don't know why this behavior. SPI signal levels should not decrease like that. 

Read operation:

=> sf read 0x00910000 0x0 0x1000
device 0 offset 0x0, size 0x1000
SF: 4096 bytes @ 0x0 Read: OK
=>

2020-03-04-2-imx6ullcom-4_spi_nor_signals_read.jpg2020-03-04-2-imx6ullcom-4_spi_nor_clk.jpg

Comapare OCRAM write buffer vs OCRAM read buffer:

=> cmp 0x00900000 0x00910000 0x1000
word at 0x00900100 (0x123456b8) != word at 0x00910100 (0xffffffff)
Total of 64 word(s) were the same
=>

64 words are ok, the rest not. 

Spi nor pads are configured this way:

#ifdef CONFIG_SYS_USE_SPINOR
static iomux_v3_cfg_t const ecspi1_pads[] = {
_MX6_PAD_CSI_DATA06__ECSPI1_MOSI | MUX_PAD_CTRL(SPI_PAD_CTRL),
_MX6_PAD_CSI_DATA04__ECSPI1_SCLK | MUX_PAD_CTRL(SPI_PAD_CTRL),
_MX6_PAD_CSI_DATA07__ECSPI1_MISO | MUX_PAD_CTRL(SPI_PAD_CTRL),

/* CS Pin */
_MX6_PAD_CSI_DATA05__GPIO4_IO26 | MUX_PAD_CTRL(NO_PAD_CTRL),
};

static void setup_spinor(void)
{
imx_iomux_v3_setup_multiple_pads(ecspi1_pads, ARRAY_SIZE(ecspi1_pads));
gpio_direction_output(IMX_GPIO_NR(4, 26), 0);
}

Best regards

Carlos

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
4,505 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Carlos

regarding "signal levels" one can try to incresae drive strength

MX6_PAD_CSI_DATA pads using DSE field in IOMUXC_SW_PAD_CTL_PAD

registers, like in sect.32.6.257 SW_PAD_CTL_PAD_CSI_DATA06 SW PAD Control
Register (IOMUXC_SW_PAD_CTL_PAD_CSI_DATA06)

i.MX 6ULL Applications Processor Reference Manual

also one can check with oscillocope power supplies spi-nor flash and NVCC_CSI

power which supplies these pads according to Table 91. 14 x 14 mm Functional Contact Assignments

i.MX 6ULL Applications Processors for Consumer Products

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
4,505 次查看
carbar
Contributor I

Hello Igor, 

we had a error in our design and for some reason the resistor that  connects  NVCC_CSI  to DCDC_3V3 (from PMIC ) was not present. Now read/write to spi nor is working ok, and booting from spi nor too.

Thanks

Carlos

0 项奖励
回复
4,506 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Carlos

regarding "signal levels" one can try to incresae drive strength

MX6_PAD_CSI_DATA pads using DSE field in IOMUXC_SW_PAD_CTL_PAD

registers, like in sect.32.6.257 SW_PAD_CTL_PAD_CSI_DATA06 SW PAD Control
Register (IOMUXC_SW_PAD_CTL_PAD_CSI_DATA06)

i.MX 6ULL Applications Processor Reference Manual

also one can check with oscillocope power supplies spi-nor flash and NVCC_CSI

power which supplies these pads according to Table 91. 14 x 14 mm Functional Contact Assignments

i.MX 6ULL Applications Processors for Consumer Products

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------