imx6ull wdt reset occurs continuously even after clear and reset cpu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull wdt reset occurs continuously even after clear and reset cpu

717 Views
titusstalin
Contributor V

Hi,

I'd generated the WDT reset by kernel panic and uboot detects the WDT reset correctly but after clearing the bit (SRC_SRSR.wdog_rst_b) and reset, still WDT is occurring till I do power cycle. i.e after power cycle it was proper.

What could be the issue ?

U-Boot 2020.04-5.10.9-1.0.0+gad7247c882 (Jan 14 2023 - 14:30:11 +0530)

CPU:   i.MX6ULL rev1.1 528 MHz (running at 396 MHz)
CPU:   Industrial temperature grade (-40C to 105C) at 48C
Reset cause: WDOG
Model: i.MX6 ULL 14x14 EVK Board
Board: MX6ULL 14x14 EVK
DRAM:  512 MiB
NAND:  0 MiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0 (480 x 272)
In:    serial
Out:   serial
Err:   serial
switch to partitions #0, OK
mmc1(part 0) is current device
flash target is MMC:1
Net:   
Warning: ethernet@2188000 (eth0) using random MAC address - 62:4c:7e:4a:93:16
eth0: ethernet@2188000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot:  0 
=> 
=> 
=> md 0x20D8008 1
020d8008: 00000010                               ....
=> 
020d800c: 00000000                               ....
=> md 0x20D8008 1
020d8008: 00000010                               ....
=> mw 0x20D8008 0x10
=> md 0x20D8008 1   
020d8008: 00000000                               ....
=> reset
resetting ...


U-Boot 2020.04-5.10.9-1.0.0+gad7247c882 (Jan 14 2023 - 14:30:11 +0530)

CPU:   i.MX6ULL rev1.1 528 MHz (running at 396 MHz)
CPU:   Industrial temperature grade (-40C to 105C) at 48C
Reset cause: WDOG
Model: i.MX6 ULL 14x14 EVK Board
Board: MX6ULL 14x14 EVK
DRAM:  512 MiB
NAND:  0 MiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0 (480 x 272)
In:    serial
Out:   serial
Err:   serial
switch to partitions #0, OK
mmc1(part 0) is current device
flash target is MMC:1
Net:   
Warning: ethernet@2188000 (eth0) using random MAC address - 32:61:c0:6a:fc:a6
eth0: ethernet@2188000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot:  0 
=> 
=> 
=> 
=> md 0x20D8008 1
020d8008: 00000010                               ....
=> 

 

titusstalin_0-1677000194756.png

 

 

Labels (4)
0 Kudos
3 Replies

676 Views
titusstalin
Contributor V

Steps to reproduce the issue:

1. Boot Linux OS

2. Create kernel panic

3. WDT reset occured

4. Rebooted automatically to Linux OS again

5. Dump SRC_SRSR register and can see WDT event, and clear it (which is expected)

6. Do 'reboot' command

7. Linux OS booted

8. Dump SRC_SRSR register and can see WDT event again which is unexpected.

9. Press reset button or power cycle the board

10. Now WDT event got cleared.

 

0 Kudos

689 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You need to download the proper dirver for wdt, since you are playing with a non-supported kernel version is probably that you don't have the driver, please download an official bsp from:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Regards

 

0 Kudos

681 Views
titusstalin
Contributor V

Thanks for your reply.

I am using official kernel release from nxp and wdt driver is used from below location.

<linux>/drivers/watchdog/imx2_wdt.c

Tags (1)
0 Kudos