imx6ull 's gpio_dvfs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ull 's gpio_dvfs

3,211 次查看
changbaoma
Contributor IV

Hi, Experts

below is imx6ull evk's Schematic

pastedImage_1.png

GPIO_DVFS & PMIC_STBY_REQ are used to select the voltage of VDD_ARM_SOC_IN. As i know PMIC_STBY_REQ is the dedicated pin, but i do know where and how this GPIO_DVFS is used in imx6ull BSP's kernel? and i can't even find out any description in dts?

Any suggest is appreciated!

标签 (1)
标记 (2)
0 项奖励
回复
7 回复数

2,934 次查看
igorpadykov
NXP Employee
NXP Employee

Hi changbao

one can check description in sect.2.5.3 CPU Frequency Scaling (CPUFREQ)

Linux Manual included in Linux 4.19.35_1.1.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,934 次查看
changbaoma
Contributor IV

Hi igorpadykov

Think you for your reply.

        I have read through the Chapter 2.5.3 CPU Frequency Scaling (CPUFREQ) , but it do not answer my question. As i know GPIO_DVFS  is a gpio, so i think this gpio must be controlled by a driver in somewhere in the kernel.  So my question is how can i find this driver and code related to GPIO_DVFS?

BTW:

i noticed someone post in this community

https://community.nxp.com/message/1246207?commentID=1246207#comment-1246207 

reg_gpio_dvfs: regulator-gpio {
   compatible = "regulator-gpio";
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_dvfs>;
   regulator-min-microvolt = <1300000>;
   regulator-max-microvolt = <1400000>;
   regulator-name = "gpio_dvfs";
   regulator-type = "voltage";
   gpios = <&gpio5 3 GPIO_ACTIVE_HIGH>;   /* This gpio match the GPIO_DVFS in imx6ull evk */
   states = <1300000 0x1 1400000 0x0>;
};

&cpu0 {
dc-supply = <&reg_gpio_dvfs>;
};

but i can't find this reg_gpio_dvfs node in kernel dts directory.

0 项奖励
回复

2,934 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

2,934 次查看
changbaoma
Contributor IV

Thanks a lot, igorpadykov

You the kernel version metioned above is v4.19.35

My project use a newer kernel version v4.19.56 @ imx6ull-14x14-evk.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

,which do not have reg_gpio_dvfs node define  in dts.

Is that mean the  kernel v4.19.56 or later version do not support  VDD_ARM_SOC_IN  voltage select by GPIO_DVFS?

pastedImage_3.png

or the  kernel v4.19.56 controll this GPIO_DVFS by other method?

Best Regards,

0 项奖励
回复

2,934 次查看
igorpadykov
NXP Employee
NXP Employee

kernel v4.19.56 is not supported by nxp, please post issue

on meta-freescale@lists.yoctoproject.org | Home 

Supported kernels are listed on i.MX Software and Development Tools | NXP 

Best regards
igor

0 项奖励
回复

2,934 次查看
changbaoma
Contributor IV

Hi, igorpadykov

when click the “Source Code” below,

pastedImage_2.png

it auto jump to Code Aurora git repositories.

How can i git pull the Linux 4.19.35_1.1.0 source code?

Can you show me the full cmd name to git pull?

0 项奖励
回复

2,934 次查看
igorpadykov
NXP Employee
NXP Employee

please check Linux 4.19.35_1.1.0 Documentation

Best regards
igor

0 项奖励
回复