imx6ull failed to interface TJA1100 transmit clk/data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull failed to interface TJA1100 transmit clk/data

Jump to solution
1,857 Views
daeyunhan
Contributor II

Hi,

I'm trouble in interfacing between FEC and TJA1100 phy.

my test environment is:

- i.mx6ull

- linux 4.9.11

- MII mode ( 4bits data, 100M duplex, 25MHz txc/rxc as separate clock)

with current driver, receive part is working well from PC to RAD Moon(Signal converter) to target board.

when PC side sends ping command to target board, it responds to ping command properly by checking data  with tcpdump tool. and target board side shows ping reply response correctly, but actual transmission failed to reply ping for PC side. that's why transmission data is not working well from FEC to Phy.

I've captured some waveforms by using CRO.

FEC test environment is:

- tx data: data 10 alternate , for example, 10100101( 0x5a)

- digital loopback(PCS block) in TJA1100

- txd pin, rxd pin captured by CRO

if data can be generated 1010 alternate at FEC side, drivers/net/ethernet/freescale/fec_main.c, I could see data at each TXD0,1,2,3. 

as you see, tx data seems to be fed into phy without problem, but the resultant digital loopback data are shown some 1s string and other 0s except single normal output.

[FEC TX data from imx6ull ]

pastedImage_1.jpg

[RX data from phy after digital loopback]

pastedImage_2.jpg

and I've tried to narrow down this problem in terms of tx data and tx clock.

data is clocked on rising edge for 10M/100Mbps. strangely,  data 10 alternate was generated on rising and falling edge synchronous. I've tried to look at reference manual and fec_main.c, failed to fix it except FEC_QUIRK_HAS_GBIT at fec_main.c. that's why 1GBS data is clocke on both(falling/rising)edge synchronously.

here's the problematic waveform by CRO

- yellow line: tx clock

- green line: tx data

[all 1's data captured at Phy side, though tx data 10 alternate  transmitted at FEC side]

pastedImage_3.jpg

[all 0's data captured at Phy side, though tx data 10 alternate  transmitted at FEC side]

pastedImage_4.jpg

do you have patch driver for fixing it up?

please, refer to current fec driver as attached( linux4.9.11 )

Thanks in advance.

0 Kudos
1 Solution
1,321 Views
daeyunhan
Contributor II

Hi Igor,

due to your support, this issue has been resolved!.

my target board with i.mx6ull has used reference linux source code with KSZ8081( reference phy device).

this ethernet phy device works on RMII(50MHz), but I use TJA1100 as MII(25MHz).

linux/drivers/clk/imx/clk-imx6ul.c:

clk_set_rate(clks[IMX6UL_CLK_ENET_REF],50000000);

==>

clk_set_rate(clks[IMX6UL_CLK_ENET_REF],25000000);

now, after fix up, ping test is working well.

Thanks again,

DaeYun.

View solution in original post

0 Kudos
6 Replies
1,322 Views
daeyunhan
Contributor II

Hi Igor,

due to your support, this issue has been resolved!.

my target board with i.mx6ull has used reference linux source code with KSZ8081( reference phy device).

this ethernet phy device works on RMII(50MHz), but I use TJA1100 as MII(25MHz).

linux/drivers/clk/imx/clk-imx6ul.c:

clk_set_rate(clks[IMX6UL_CLK_ENET_REF],50000000);

==>

clk_set_rate(clks[IMX6UL_CLK_ENET_REF],25000000);

now, after fix up, ping test is working well.

Thanks again,

DaeYun.

0 Kudos
1,321 Views
daeyunhan
Contributor II

i.MX6ULL EVK doesn't have any TJA1100 phy driver in terms of ethernet interface.

instead, I've summarized this FEC issue as follows.

1. FEC interface

- 4 bits TX Data: TXD[0...3] as FEC --> TJA1100

- TXC: tx clock(25MHZ)      as  FEC <-- TJA1100

pastedImage_1.png

this FEC data should be transmitted according to TXC(tx clock) generated by TJA1100.

i.mx6ull reference manual has also this description(IMX6ULLRM.pdf):

TX data are synchronous to TX Clock rising edge

pastedImage_2.png

additionally, TJA1100 has also the same behaviour:

TJA1100 expects that FEC data should be synchronous to TX Clock rising edge as well.

pastedImage_1.png

pastedImage_6.png

2. FEC/PHY Timing diagram

2.1 the expected and ideal behaviour btw FEC tx data and TJA1100 tx clock

if you would send 101010..... data, you must see tx clock and tx data,

that is, TXD data value can be changed to TX clock rising edge as follows:

pastedImage_7.png

2.2 the actual & problematic behaviour btw FEC tx data and TJA1100 tx clock.

actual tx data value was changed to TX clock rising/falling edge with 101010.... data sequence.

TJA1100 must see this TX data as all 1's all the time.

pastedImage_9.png

3. DTS data for IOMUX pins.

- 4 bits tx data

- tx clcok

- 4 bits rx data

- rx clcok

pinctrl_enet1: enet1grp {
fsl,pins = <
MX6UL_PAD_ENET1_RX_EN__ENET1_RX_EN 0x1b0b0
MX6UL_PAD_ENET1_RX_ER__ENET1_RX_ER 0x1b0b0
MX6UL_PAD_ENET1_RX_DATA0__ENET1_RDATA00 0x1b0b0
MX6UL_PAD_ENET1_RX_DATA1__ENET1_RDATA01 0x1b0b0
MX6UL_PAD_UART1_TX_DATA__ENET1_RDATA02 0x1b0b0
MX6UL_PAD_UART1_RX_DATA__ENET1_RDATA03  0x1b0b0
MX6UL_PAD_UART1_CTS_B__ENET1_RX_CLK 0x4001b031
MX6UL_PAD_ENET1_TX_EN__ENET1_TX_EN 0x1b0b0
MX6UL_PAD_UART1_RTS_B__ENET1_TX_ER 0x1b0b0
MX6UL_PAD_ENET1_TX_DATA0__ENET1_TDATA00 0x1b0b0
MX6UL_PAD_ENET1_TX_DATA1__ENET1_TDATA01 0x1b0b0
MX6UL_PAD_UART2_TX_DATA__ENET1_TDATA02 0x1b0b0
MX6UL_PAD_UART2_RX_DATA__ENET1_TDATA03 0x1b0b0
MX6UL_PAD_ENET1_TX_CLK__ENET1_TX_CLK 0x4001b031
>;
};
4. RX data test is always OK, but TX data is always broken due to TX Clock synchronization.
I've checked tx clock synchronization register for adjusting data output timing like hold time and rising or falling edge,
but failed to find out the initialization code at drivers/net/ethernet/freescale/fec_main.c
additionally, i.mx6ul(l) reference manual doesn't have any explanation for tx data/clock synchronization control/monitoring more.
this FEC driver seems to act on 1G ethernet, that is, TX data output is synchronous to rising and falling both of them.
like 10M/100Mbps, TX data output should be synchronous to only rising edge, one of them.
please, check how to change tx, rx clock& data sync independently in similar i.mx6ull or i.mx6sx or i.mx6ul chip.
if there's patch driver for this issue, it'll big helpful.
Thanks and Regards.
Daeyun.
0 Kudos
1,321 Views
igorpadykov
NXP Employee
NXP Employee

if you think that problem in FEC driver, this should not depend on TJA1100 phy
or any other external chip. Specific software changes for TJA1100 can be found in:

linux.git - Automotive Linux Tree 

You can use NXP Professional Services for getting help with developing this custom driver:
NXP Professional Services|NXP 

Best regards
igor

0 Kudos
1,321 Views
daeyunhan
Contributor II

Hi Igorpadykov,

this problem depends on FEC driver rather than Phy driver.

Phy device generates 25MHz tx clock properly, and FEC data should sends tx data[0..3] on tx clock rising edge.

but actually imx6ull FEC device now outputs tx data on both falling/rising edge like 1000 Mbps link speed.

here's my ported driver for linux version 4.9.11

though FEC problem, now, I've tried to slow down the link speed from 100 Mbps to 10 Mbps in phy driver.

I expected that 100 Mbps mode has 25MHz tx clock and 10 Mbps mode has 2.5MHz tx clock.

but after changing to 2.5MHz tx clock, I've checked actual tx clock and tx clock showed 25MHz instead of 2.5MHz

can TJA1100 change the link speed from 25MHz to 2.5 MHz in terms of 10 Mbps speed?

here's phy driver mode:

- managed mode

- 10Mbps

- Basic control register: tried to set register with 00(10Mbps), 01(100Mbps)

/* Configures the autonegotiation capabilities */
static int nxp_config_aneg(struct phy_device *phydev)
{
if (verbosity > 0)
phydev_err(phydev, "configuring autoneg\n");

/* disable autoneg and manually configure speed, duplex, pause frames */
phydev->autoneg = 0;

phydev->speed = SPEED_100; // <- can be changed with SPEED_10
phydev->duplex = DUPLEX_FULL;

phydev->pause = 0;
phydev->asym_pause = 0;

return 0;
}

0 Kudos
1,321 Views
igorpadykov
NXP Employee
NXP Employee

if you think that problem in FEC driver, could you try

to reproduce issue on i.MX6ULL EVK with NXP Demo images

https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_iMX6UL7D&appType=license&location=null 

Best regards
igor

0 Kudos
1,321 Views
igorpadykov
NXP Employee
NXP Employee

Hi DaeYun

please look at driver sources for this chip and add necessary changes to

custom codes

linux.git - Automotive Linux Tree 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos