imx6ull MCIMX6Y7DVM09AB chip ethernet not work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ull MCIMX6Y7DVM09AB chip ethernet not work

1,688 次查看
chenfeng2016
Contributor I
Hello, about imx6ull, I have a question about Ethernet  need your help
 
In our project, when using imx6ull MCIMX6Y2CVM08AB chip, the ethernet  network can work normally.  you can see eth0 and eth1, by  ifconf -a ,but  the same hardware is replaced with imx6ull chip to MCIMX6Y7DVM09AB, the Ethernet network does not work, and eth0 or eth1 cannot be seen by  ifconfig -a 
 
Help to analyze the causes, thanks
 
 MCIMX6Y2CVM08AB and MCIMX6Y7DVM09AB boot log attached.
标签 (1)
0 项奖励
回复
1 回复

1,668 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The two chip have some difference,the MCIMX6Y7DVM09AB only support one Ethernet, and the MCIMX6Y2CVM08AB  support Ethernet x2.

 

0 项奖励
回复