imx6ull 524Mhz GPMI interface NAND speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull 524Mhz GPMI interface NAND speed

1,906 Views
dc1
Contributor II

Hello all, 

i have a imx6ull 524Mhz cpu connected with the interface GPMI to a NAND MT29F32G08CBADBWP in EDO mode 5:

gpmi-nand 1806000.gpmi-nand: enable the asynchronous EDO mode 5

with ubifs (an old version ... 2017)

My gpmi device tree is set as:

&gpmi {

compatible = "fsl,imx6ull-gpmi-nand", "fsl, imx6ul-gpmi-nand";
#address-cells = <1>;
#size-cells = <1>;
reg = <0x01806000 0x2000>, <0x01808000 0x4000>;
reg-names = "gpmi-nand", "bch";
interrupts = <GIC_SPI 15 IRQ_TYPE_LEVEL_HIGH>;
interrupt-names = "bch";
clocks = <&clks IMX6UL_CLK_GPMI_IO>,
<&clks IMX6UL_CLK_GPMI_APB>,
<&clks IMX6UL_CLK_GPMI_BCH>,
<&clks IMX6UL_CLK_GPMI_BCH_APB>,
<&clks IMX6UL_CLK_PER_BCH>;
clock-names = "gpmi_io", "gpmi_apb", "gpmi_bch",
"gpmi_bch_apb", "per1_bch";
dmas = <&dma_apbh 0>;
dma-names = "rx-tx";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_gpmi_nand_1>;
status = "okay";
nand-on-flash-bbt;
};

my speed test show this result :

dd if=/dev/zero of=./largefile bs=1M count=1024

1073741824 bytes (1.1 GB, 1.0 GiB) copied, 47.6832 s, 22.5 MB/s

dd if=/dev/zero of=./largefile bs=1M count=1024 oflag=dsync

1073741824 bytes (1.1 GB, 1.0 GiB) copied, 50.2484 s, 21.4 MB/s

dd if=/dev/zero of=./largefile bs=100M count=10

1048576000 bytes (1.0 GB, 1000 MiB) copied, 42.4279 s, 24.7 MB/s

dd if=/dev/zero of=./largefile bs=100M count=10 oflag=dsync

1048576000 bytes (1.0 GB, 1000 MiB) copied, 50.4285 s, 20.8 MB/s

My question is if it is possible to increase the gpmi frequency clock to reach better speed performance and, in case, how to do that?

Can you help me?

Thanks

Labels (2)
0 Kudos
Reply
1 Reply

1,852 Views
igorpadykov
NXP Employee
NXP Employee

Hi Daniele

>My question is if it is possible to increase the gpmi frequency clock..

I am afraid it is not possible and gpmi (nand) driver selects operating frequency

automatically, one can refer to driver source comments:

4.4) We only support the fastest asynchronous mode of ONFI nand.
 *       For some ONFI nand, the mode 4 is the fastest mode;
 *       while for some ONFI nand, the mode 5 is the fastest mode.
..
The async mode requires 40MHz for mode 4, 50MHz for mode 5.

gpmi-lib.c\gpmi-nand\nand\mtd\drivers - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------