imx6ull 工业级在80度高温测试会 power down,请问下是否正常

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull 工业级在80度高温测试会 power down,请问下是否正常

1,321 Views
michael_yang
Contributor II

imx6ull MCIMX6Y2CVM05AB 工业级在80度高温测试会 power down, 芯片规格书写了Temperature
Tj -40 to 105

0 Kudos
Reply
6 Replies

1,279 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @michael_yang,

I hope you are doing well.

Could you confirm if the 80 degrees is the ambient temperature or the processor's junction temperature?

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply

1,274 Views
michael_yang
Contributor II

Hi Team, 

80 degrees is the ambient temperature

0 Kudos
Reply

1,265 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @michael_yang,

Thanks for the confirmation.

Since 80 degrees is the ambient temperature, please share the logs of the processor before it shut down, mentioning the junction temperature of the processor.
I expect the junction temperature to be pretty more at 80 degrees of ambient temperature.

One can print the junction temperature of the processor continuously on the console by using the below-mentioned command:
cat /sys/devices/virtual/thermal/thermal_zone0/temp

Thanks & Regards,
Ritesh M Patel 

0 Kudos
Reply

1,239 Views
michael_yang
Contributor II

Hi @riteshmpatel

we look at log cat /sys/devices/virtual/thermal/thermal_zone0/temp, and running at 80 degrees for 10 minutes, there is a power down, junction temperature is close to 105 degrees, is it a hardware problem?

Tags (1)
0 Kudos
Reply

1,211 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @michael_yang,

Apologies for the delay in response.

The junction temperature will always be greater than the ambient temperature.

To calculate Tj(Junction temperature) you need to use the equation Tj = Ta + ( RθJA * PD ).

Ta = Ambient temperature

RθJA = Junction to ambient thermal resistance (51.4 °C/W)

PD = Power dissipation (Vout * Iout)

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply

1,196 Views
smithcoba
Contributor III

@riteshmpatel 

The cat /sys/devices/virtual/thermal/thermal_zone0/temp is already the temperature from  junction.

Your formula is thermal resistance to estimate  junction temperature.

For example, know the  Ambient and the power, then you can calculate/estimate the junction temperature.

Untitled.png

So far, at this moment, is to check the passive and critical settings. 

cat /sys/devices/virtual/thermal/thermal_zone0/trip_point_?_*
2000
85000
passive
2000
95000
critical

0 Kudos
Reply