Hello,
I tried some test about compiling kernel with cross-compiler tools. I burned those files to the sdcard and it could successfully start u-boot. But it get stuck when it start with kernel. And I used the
The log's picture is as follows:
How can I deal with it ? Hope your help. Thanks !
Hi Ida
from log "Can not find fsl,optee-lpm-sram node in the device tree", one can try to
disable optee using sect.5.6.10 OP-TEE enablement attached Yocto Guide
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor ,
Sorry for the late reply, and I really thank you for your reply to my question.
I think you are right. I tried to disable the optee and did it again. The board could boot normally.
And thank you again for your help.
Best Regards!
Ida
发件人: igorpadykov
发送时间: 2019年10月15日 8:26
收件人: Ida Jiang 江一
主题: Re: - Re: imx6ulevk get stuck when it start with kernel
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: imx6ulevk get stuck when it start with kernel
reply from igorpadykov<https://community.nxp.com/people/igorpadykov?et=watches.email.thread> in i.MX Processors - View the full discussion<https://community.nxp.com/message/1218635?commentID=1218635&et=watches.email.thread#comment-1218635>