imx6ulevk get stuck when it start with kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ulevk get stuck when it start with kernel

731 Views
ida_jiang
Contributor III

Hello,

     I tried some test about compiling kernel with cross-compiler tools. I burned those files to the  sdcard and it could successfully start u-boot. But it get stuck when it start with kernel. And I used the 

    The log's picture is as follows:

内核卡住.png

How can I deal with it ? Hope your help. Thanks !

Tags (2)
0 Kudos
2 Replies

681 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ida

from log "Can not find fsl,optee-lpm-sram node in the device tree", one can try to

disable optee using sect.5.6.10 OP-TEE enablement attached Yocto Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

681 Views
ida_jiang
Contributor III

Hi igor ,

Sorry for the late reply, and I really thank you for your reply to my question.

I think you are right. I tried to disable the optee and did it again. The board could boot normally.

And thank you again for your help.

Best Regards!

Ida

发件人: igorpadykov

发送时间: 2019年10月15日 8:26

收件人: Ida Jiang 江一

主题: Re: - Re: imx6ulevk get stuck when it start with kernel

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: imx6ulevk get stuck when it start with kernel

reply from igorpadykov<https://community.nxp.com/people/igorpadykov?et=watches.email.thread> in i.MX Processors - View the full discussion<https://community.nxp.com/message/1218635?commentID=1218635&et=watches.email.thread#comment-1218635>

0 Kudos