imx6ul: yocto how can i update the kernel source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6ul: yocto how can i update the kernel source

ソリューションへジャンプ
1,698件の閲覧回数
半醒的狐狸
Contributor I

hi

the kernel  source i have use  is 3.14.38  in the yocto project.

but i want to use 3.14.52-1.1.0.

how?

thanks!

ラベル(3)
0 件の賞賛
返信
1 解決策
1,423件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hello

recommended to make fresh build in new folder, for

steps please refer to sect.5.3 Building an image

attached Yocto Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,424件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hello

recommended to make fresh build in new folder, for

steps please refer to sect.5.3 Building an image

attached Yocto Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信