imx6ul: yocto how can i update the kernel source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6ul: yocto how can i update the kernel source

跳至解决方案
1,702 次查看
半醒的狐狸
Contributor I

hi

the kernel  source i have use  is 3.14.38  in the yocto project.

but i want to use 3.14.52-1.1.0.

how?

thanks!

标签 (3)
0 项奖励
回复
1 解答
1,427 次查看
igorpadykov
NXP Employee
NXP Employee

Hello

recommended to make fresh build in new folder, for

steps please refer to sect.5.3 Building an image

attached Yocto Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,428 次查看
igorpadykov
NXP Employee
NXP Employee

Hello

recommended to make fresh build in new folder, for

steps please refer to sect.5.3 Building an image

attached Yocto Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复