imx6ul: yocto how can i update the kernel source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul: yocto how can i update the kernel source

Jump to solution
1,614 Views
半醒的狐狸
Contributor I

hi

the kernel  source i have use  is 3.14.38  in the yocto project.

but i want to use 3.14.52-1.1.0.

how?

thanks!

Labels (3)
0 Kudos
Reply
1 Solution
1,339 Views
igorpadykov
NXP Employee
NXP Employee

Hello

recommended to make fresh build in new folder, for

steps please refer to sect.5.3 Building an image

attached Yocto Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,340 Views
igorpadykov
NXP Employee
NXP Employee

Hello

recommended to make fresh build in new folder, for

steps please refer to sect.5.3 Building an image

attached Yocto Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply