imx6ul with 10.1 LVDS inch display

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ul with 10.1 LVDS inch display

2,260 次查看
sarathak
Contributor I

Dear All,

I am new to BSP development in ,@imx6ul som. 

We are planning to use 10.1 inch LVDS display in I.MX6-UL based SOM,  

Please suggest me its is possible or not, If possible how to do this, 

Kindly help us.

0 项奖励
回复
2 回复数

1,797 次查看
embedded_Dev
Contributor III

Hello sarathak,

Can you please share the dtsi file for reference. I am using 7 inch LVDS LCD but i cant able to see anything on the screen. Can you please share ASAP.

Thank You

0 项奖励
回复

1,911 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sarath

lvds lcds are not natively supported by i.MX6UL (there is no LDB module),

one can use some converter (parallel to lvds output) like DS90C385AMT or similar.

Note, also one will have to develop driver for it. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复