imx6ul.the dts about the weim

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul.the dts about the weim

2,361 Views
半醒的狐狸
Contributor I

hi

i went to use the weim driver,but i dont't know who to config the dts.

the kernel document have gave a Example:(kernel-source\Documentation\devicetree\bindings\bus\imx-weim.txt).

Example for an imx6q-sabreauto board, the NOR flash connected to the WEIM:

  weim: weim@021b8000 {

  compatible = "fsl,imx6q-weim";

  reg = <0x021b8000 0x4000>;

  clocks = <&clks 196>;

  #address-cells = <2>;

  #size-cells = <1>;

  ranges = <0 0 0x08000000 0x08000000>;

  nor@0,0 {

  compatible = "cfi-flash";

  reg = <0 0 0x02000000>;

  #address-cells = <1>;

  #size-cells = <1>;

  bank-width = <2>;

  fsl,weim-cs-timing = <0x00620081 0x00000001 0x1c022000

  0x0000c000 0x1404a38e 0x00000000>;

  };

  };

mine :

weim: weim@021b8000 {

  compatible = "fsl,imx6ul-weim", "fsl,imx6q-weim";

  reg = <0x021b8000 0x4000>;

  interrupts = <GIC_SPI 14 IRQ_TYPE_LEVEL_HIGH>;

  clocks = <&clks IMX6UL_CLK_EIM_SLOW_PODF>;

  };    //int the imx6ul.dtsi

&weim {

  pinctrl-names = "default";

  pinctrl-0 = <&pinctrl_weim>;

  #address-cells = <2>;

  #size-cells = <1>;

  status = "okay";

  ranges = <0 0 0x50000000 0x08000000>;

  imx-weim@0,0 {

  compatible = "imx-weim";

  reg = <0 0 0x02000000>;

  #address-cells = <1>;

  #size-cells = <1>;

  bank-width = <2>;

  fsl,weim-cs-timing = <0x403304b1 0x00000001 0x0f010000

  0x00000008 0x0f040040 0x00000000>;

  };

};   //in the imx6ul-14x14-evk.dts

pinctrl_weim: weimgrp {

  fsl,pins = <

  MX6UL_PAD_CSI_MCLK__EIM_CS0_B   0x10b0

  MX6UL_PAD_CSI_PIXCLK__EIM_OE   0x10b0

  MX6UL_PAD_CSI_VSYNC__EIM_RW 0x10b0 

  MX6UL_PAD_LCD_DATA08__EIM_DATA00 0x1b0b0

  ...

  ....

  >;

  };   //in the imx6ul-14x14-evk.dts

but i can't read the register and ioremap the weim memory.

@igorpadykov

tolt me i can check the CCM register CCM_CCGR6  . imx6ul:help,i can't read or write the weim  register​.

when i changed the value ,i can read and write the memory.

thanks again .

but wen i use the  oscilloscope to check the wei.cs0 、wei.oe 、wei.rw 

No matter how many times to read   ,they only change once ,and can't read or write the real value.

In my mind,if the kernel  afford the driver ,i only change the dts if i want to use the  driver .for example the ecspi ,i2c driver. but in this  mode ,i can't read the memory  if i didn't change the  CCM register CCM_CCGR6  .

i thank it's not the normal way to use this driver.

i can't find any more information form the kernel except the  Example for an imx6q-sabreauto board(kernel-source\Documentation\devicetree\bindings\bus\imx-weim.txt).

Some people tolt me i only to config the dts.and ioremap the 5000_0000 memory  phy_adr to read and write.

but i don't know how to config the dts in right way.

the Example  in the kernel Documentation  is  right?

why i have to config the   CCM register CCM_CCGR6  even i have  configed the dts Modelled on the Example  ,if i want to read or write the memory.

Thank you for attention!!

Labels (2)
0 Kudos
Reply
2 Replies

1,075 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yi

I think it is not possible to enable CCM_CCGRn in dts, however

one can try to set it in dcd header (uboot *.cfg init file)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,075 Views
半醒的狐狸
Contributor I

Hi igor

    sorry ,i don't know who to find the dcd header,but i know the problem may be in tne kernel .

i modify the weim driver,add same debugging information:

#define  CLK_register     0x20C4080

    struct resource  *my_mem ;

    int offset = 0;

    printk("offset = %d\n",offset);

    my_mem = request_mem_region(CLK_register + 0x4000 * offset, 0x4000, "testPF");

    if (my_mem == NULL) {

        printk("failed to get memory region\n");

        return -ENOENT;

    } else

        printk("phy_addr = %08x\n",CLK_register + 0x4000 * offset);

    void __iomem    *plx_membase ;

    plx_membase = ioremap(CLK_register + 0x4000 * offset, 0x4000);      

    if(NULL == plx_membase) {

        printk("ioremap error\n");

    }

    printk("ioremap_addr=%lx\n",(u_long)plx_membase);    

    printk("print_out: %08x\n",readl(plx_membase));       

    printk("+++++++++++++++++++++\n");

    unsigned int ret_val = readl(plx_membase);

    ret_val = ret_val | ( 0x3 <<  10);

    writel(ret_val ,plx_membase);

    printk("print_out: %08x\n",readl(plx_membase));        

    iounmap(plx_membase);

    release_mem_region(CLK_register + 0x4000 * offset,0x4000);

when the board staring:

加载信息.png

but after logo ,the CCM register CCM_CCGR6 have been modified.and i can't read or write the weim register......

by other way,i can use the weim by using my driver to init  the   CCM register CCM_CCGR6.

ioremap the phy_adr by " /dev/mem."

and it work well.

tek00002.png

how can i find the clk init function?

thanks!

0 Kudos
Reply