imx6ul systemd waiting for ttymxc0 failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul systemd waiting for ttymxc0 failed

4,485 Views
xiongjunhe
Contributor II

I use the systemd initialization manager to booting  the system, but it cann't enter the Getty for waiting for ttymxc0 timeout (using the serial):

[  OK  ] Started Authorization Manager.
[  OK  ] Started Getty on tty1.
[  OK  ] Started Modem Manager.
[  OK  ] Created slice system-sshd.slice.
[  OK  ] Started OpenSSH Per-Connection Daemon (192.168.1.106:38772).
[ TIME ] Timed out waiting for device dev-ttymxc0.device.
[DEPEND] Dependency failed for Serial Getty on ttymxc0.
[  OK  ] Reached target Login Prompts.
[  OK  ] Reached target Multi-User System.
         Starting Update UTMP about System Runlevel Changes...
[  OK  ] Started Update UTMP about System Runlevel Changes.‍‍‍‍‍‍‍‍‍‍‍

But I can get into the console through ssh, also, I can get into the getty when using the init.d instead of systemd so the ttymxc0 is fine, but it just wouldn't be detected by the systemd, maybe the udev is the fault?

And the system is build using the yocto. The udevd is running.

# udevadm info /dev/ttymxc0
P: /devices/platform/soc/2000000.aips-bus/2000000.spba-bus/2020000.serial/tty/ttymxc0
N: ttymxc0
E: DEVNAME=/dev/ttymxc0
E: DEVPATH=/devices/platform/soc/2000000.aips-bus/2000000.spba-bus/2020000.serial/tty/ttymxc0
E: ID_MM_CANDIDATE=1
E: MAJOR=207
E: MINOR=16
E: SUBSYSTEM=tty
E: TAGS=:systemd:
E: USEC_INITIALIZED=11599104

I can see the udev service is started:

[  OK  ] Started udev Kernel Device Manager.
         Starting Update UTMP about System Boot/Shutdown...
         Starting Network Time Synchronization...
[  OK  ] Started Update UTMP about System Boot/Shutdown.

Also I tried to trigger a event in ssh durning the systemd is waiting for the ttymxc0, but no luck:

udevadm trigger -v --type subsystems --action add -s tty --sysname-match=ttymxc0
Labels (1)
Tags (2)
6 Replies

2,486 Views
stuartmorton
Contributor II

Hi, I'm having exactly the same issue. Did you manage to fix it?

I've asked mr google and found people saying that you have to have FHANDLE=y and IKCONFIG=y configured in the kernel but I've tried this and ti doesn't solve my problem.

Thanks.

0 Kudos

2,486 Views
xabiermarquiegu
Contributor II

Hello. I am having the same issue. Have you managed to find a solution? I also have FHANDLE, and IKCONFIG on in the kernel, but this keeps happening in some conditions.

0 Kudos

2,486 Views
gaun
Contributor II

I had solved this problem with another board by enabling CONFIG_FHANDLE. What kernel are you using? Also do you have CONFIG_VT enabled?

2,486 Views
xabiermarquiegu
Contributor II

A million thanks for answering.

Yes, I have both CONFIG_FHANDLE and CONFIG_VT enabled. I have just figured out how to solve this problem in my setup.

Just in case this helps anyone else, in my case it was just a conflict between systemd and udevd.

I had some rules in udev that performed systemctl start, stop and restart of several systemd services. By adding the --no-block option I managed to avoid this problem.

0 Kudos

2,486 Views
yilingxu
Contributor III

Hi,

Could you please how to set  CONFIG_FHANDLE and CONFIG_VT enabled?

Thanks

Yiling Xu

0 Kudos

2,486 Views
igorpadykov
NXP Employee
NXP Employee

Hi XiongJun

what bsp used in the case, please try nxp releases described on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

try Demo Image

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.1_iMX6UL7D&appType=license&location=null&Pare... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos