imx6ul send flexcan data failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ul send flexcan data failed

2,109 次查看
qinghuazhu
Contributor III

I'm running Linux4.1.15 on imx6ul, compiled by yocto.And I haven't change any code.

After Linux start finished, I just execute commands as below:

root@imx6ulevk:~# canconfig can0 bitrate 500000

can0 bitrate: 500000, sample-point: 0.866

root@imx6ulevk:~# ifconfig can0 up

flexcan 2090000.can can0: writing ctrl=0x03292005

root@imx6ulevk:~# cansend can0 -i 0x750 0x40 0x01 0x3E 0x00 0x00 0x00 0x00 0x00

interface = can0, family = 29, type = 3, proto = 1

root@imx6ulevk:~#

I test CAN1_TX pin of U1201 by oscilloscope, no signal detected.

The same as CAN2_TX of U1202.

Anybody help? Thanks very much.

标签 (3)
0 项奖励
回复
2 回复数

1,586 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Qinghua

please try loopback test or two board connection as described on

How to enable CAN bus on i.MX6Q SabreSD

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,586 次查看
qinghuazhu
Contributor III

Thanks for your help!

But I'm sorry, I still don't understand. I can see can0/can1 now.

Do I have to change some code to enable flexcan now?

0 项奖励
回复