imx6ul sai timeslot issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul sai timeslot issue

485 Views
chenandy
Contributor II

Hello,

    Added an additional si32176 and 4G module on my board to sai3.

    asynchronous, TX Frame Sync Direction externally, RX Frame Sync Direction internally, TX and RX Bit Clock Direction externally.
    The first timeslot starts at the falling edge of fs, but I want to imx6ul the first timeslot starts at the rising edge of fs, what can  I do?

error.png

                                                                         this is imx6ul sai txdata timeslot

valid.png

                                                                 I expect the result

Thanks in advance,

Andy

Labels (1)
0 Kudos
1 Reply

401 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

>I want to imx6ul the first timeslot starts at the rising edge of fs, what can  I do?

there is option of changing Frame Sync Polarity using FSP bit I2Sx_TCR4 register,

other sai timings can not be changed as they defined in hardware. More details

can be found in sect.42.3.4 Frame sync configuration i.MX 6UltraLite Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------