I checked the community's questions about PPS.I can now see the output of the PPS signal via "echo 1 > /sys/class/ptp/ptpx/pps_enable", what should I do to adjust the duty cycle of 1pps on imx6ul
Solved! Go to Solution.
Hi,
Thank you for your interest in NXP Semiconductor products,
You can base in this echoing:
echo "0 0 0 1 1" > /sys/class/ptp/ptp0/period
But further documentation can be found here.
Regards
View solution in original post
hi,josephlinares
Thank you for your reply.I use echo "0 0 0 1 1" > /sys/class/ptp/ptp0/period can adjust the PPS signal cycle.
I want to adjust the high level time so that the high level time is shorter than the low level time to form a PPS cycle.Is there any way to do this?
No, it is not possible, as you saw in doc, there is not a file for duty cycle adjustment but period.
Thank you,
Hi,josephlinares
Thank you for your support.
Regards.