imx6ul keypad port wakeup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6ul keypad port wakeup

897件の閲覧回数
shammi112
Contributor I

Hello,

Can i use the imx6ul keypad  port for wake-up from standby/sleep mode ?

Could you please list out the imx6ul peripheral which can by used to

wake up imx6ul from sleep/standby mode ?

Regards,

SHAMMI

ラベル(1)
0 件の賞賛
返信
1 返信

766件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi SHAMMI

any peripheral which can produce interrupt, is capable of waking processor

from low power modes. One can look at sect.3.2 Cortex A7 interrupts i.MX6ULL Reference Manual 

http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信