imx6ul:how to get the data from usb_control_msg?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul:how to get the data from usb_control_msg?

2,506 Views
半醒的狐狸
Contributor I

hi

on pc:when i use the usb_control_msg,

usb_control_msg(dev, 0x80,0x06, 768, 0, tmp,32,10000);

in the isr_setup_packet_handler(kernel-source\drivers\usb\chipidea\udc.c)  i can get the :

__u8 request = 0x80,

__u8 requesttype = 0x06,

__u16 value = 768,

__u16 index = 0,

__u16 size = 32

by struct usb_ctrlrequest req;

but i don't know how to get the data(tmp) i  have send by usb_control_msg.

thanks!

Labels (2)
0 Kudos
Reply
3 Replies

1,874 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Could you please specify which BSP are you using? Are you using any of the existing USB Classes or are you defining a custom USB Device?

Best regards!

/Carlos

0 Kudos
Reply

1,874 Views
半醒的狐狸
Contributor I

hi
the information is that:

U-Boot 2015.04-imx_v2015.04_3.14.38_6ul_ga+g5d63276 (Aug 18 2015 - 21:32:01)

CPU:   Freescale i.MX6UL rev1.0 at 396 MHz
CPU:   Temperature 43 C
Reset cause: WDOG
Board: MX6UL 14x14 EVK
I2C:   ready
DRAM:  512 MiB

when boot up
i run this:modprobe g_serial  use_acm=0
and connect pc whith micusb.
on the pc ,i used ilbusb by Qt.
when connect the usb .i run usb_control_msg(dev, 0x80,0x06, 768, 0, tmp,32,10000);
i have analyzed the code and found that:
when i run usb_control_msg on pc .
i can get the struct usb_ctrlrequest in isr_setup_packet_handler(kernel-source\drivers\usb\chipidea\udc.c)
in the struct usb_ctrlrequest i can found the :
__u8 request = 0x80,
__u8 requesttype = 0x06,
__u16 value = 768,
__u16 index = 0,
__u16 size = 32

but i don't know hwo to get the tmp that i have send by usb_control_msg on pc.

Best regards!

0 Kudos
Reply

1,874 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

You could refer to the following links, they may provide useful information related to your issue:

[PATCH 1/4] usb: chipidea: udc: refine isr_tr_complete_handler

usb - How does libusb access kernel stuff? - Unix & Linux Stack Exchange

Linux/drivers/usb/chipidea/udc.c - Linux Cross Reference - Free Electrons

Hope this will be useful for you.

Best regards!

/Carlos

0 Kudos
Reply