imx6ul evk play music

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul evk play music

2,192 Views
caibai
Contributor III

i use imx6ul evk and yocto,

when i play music like

# gst-play xxx.mp3

and it sounds have noise.

how to solve it??

Labels (3)
0 Kudos
2 Replies

1,687 Views
igorpadykov
NXP Employee
NXP Employee

HI cai

please try commands as in attached Linux Guide sect.7.3.1.1 Audio-only playback

and use  Demo Images on:

Board Support Packages (1)

L3.14.38_iMX6UL (REV L3.14.38_6ul) New

i.MX 6UltraLite Linux Binary Demo Files and Linux BSP Documentation

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,687 Views
caibai
Contributor III

thanks for reply.

i run

# gst-launch-1.0 filesrc location=test.mp3  ! id3demux ! queue ! mpegaudioparse ! beepdec ! pulsesink

but it sound the same as i run gst-play xxx.mp3

0 Kudos