imx6ul-ddr configuration-imximage.cfg file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul-ddr configuration-imximage.cfg file

Jump to solution
3,090 Views
surendradhobale
Contributor III

Hello,

   I am working with imx6ul custom board. I have boot the device with emmc and have to initilalize the ddr.

I have seen imximage.cfg is one of the file where configurations are done.

Can anyone please give me more idea about the imximage.cfg file?

I mean which registers are their and what values i need to put ? How to modify this file if DDR coeffiecients are different?

Thanks,

Surendra 

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,238 Views
Yuri
NXP Employee
NXP Employee

Hello,

  First, please try to get the memory stress test working.

 

i.MX6/7 DDR Stress Test Tool V2.60 

   Please use the following document how to configure DDR parameters.

 

Freescale i.MX6 DRAM Port Application Guide-DDR3 

 

 As for the imximage.cfg file, please look at Chapter 1 (Porting U-Boot from
an i.MX 6/7 Reference Board to an i.MX 6/7 Custom Board) of “i.MX_BSP_Porting_Guide.pdf”.

 

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... 

 

  Also, please refer to section 8.7.2 [Device Configuration Data (DCD)] of the

i.MX6 UL RM (IMX6ULRM, Rev. 1, 04/2016)

 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

View solution in original post

0 Kudos
Reply
1 Reply
2,239 Views
Yuri
NXP Employee
NXP Employee

Hello,

  First, please try to get the memory stress test working.

 

i.MX6/7 DDR Stress Test Tool V2.60 

   Please use the following document how to configure DDR parameters.

 

Freescale i.MX6 DRAM Port Application Guide-DDR3 

 

 As for the imximage.cfg file, please look at Chapter 1 (Porting U-Boot from
an i.MX 6/7 Reference Board to an i.MX 6/7 Custom Board) of “i.MX_BSP_Porting_Guide.pdf”.

 

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... 

 

  Also, please refer to section 8.7.2 [Device Configuration Data (DCD)] of the

i.MX6 UL RM (IMX6ULRM, Rev. 1, 04/2016)

 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

0 Kudos
Reply