imx6ul can not boot from emmc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6ul can not boot from emmc

1,753件の閲覧回数
wangzhigang
Contributor III

hi everyone,
    we cann't boot from emmc (qspi,sdcard is ok),our env is :
hardware: imx6ull
emmc: SDIN7DP2-4G (4.5.1)
uboot version: imx_v2016.03_4.1.15_2.0.0_ga (mx6ull_14x14_evk_emmc_defconfig)

boot mode 1 = on
boot mode 0 = off
BOOT_CFG1[7-0] = 01110010
BOOT_CFG2[7-0] = 00000100 (eSHD2)
BOOT_CFG4[7-0] = 00000000

1、sdchard (eSHD1)and qspi is ok ,so ddr parameter must have no problem
2、could you tell me the right configs (BOOT_CFG1/BOOT_CFG2/BOOT_CFG4) when boot from emmc.

we found there are so many people have the same problem, please give me a hand!!!
Best wishes!

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,481件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi wang

for emmc boot configs one can look at p.9 spf-28617 i.MX6UL EVK schematic

Schematics (1)
MCIMX6UL-EVK_DESIGNFILES
Design files, including hardware schematics, Gerbers, and OrCAD files.
i.MX6UltraLite Evaluation Kit|NXP 

Use mfg tool for emmc programming

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,481件の閲覧回数
wangzhigang
Contributor III

hi, igor igorpadykov

   thanks for your answer.

   1. yes, the  MCIMX6UL-EVK is our reference board, but the demo board have no emmc instend of sd card as default. 

   2. 

    BOOT_CFG1:

pastedImage_2.png

    BOOT_CFG2:

pastedImage_1.png

      

  the emmc config is complicate, our config is :

   BOOT_CFG1[7-0] = 01110010

   BOOT_CFG2[7-0] = 00000100 (eSHD2)

  is this ok?

    

   3. we will use the mfgtools for test.

Best regards

0 件の賞賛
返信