imx6ul bitbake fsl-image-qt5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6ul bitbake fsl-image-qt5

跳至解决方案
1,636 次查看
luoyaojun
Contributor II

yocto中指定imx6ul平台使用bitbake fsl-image-qt5生成的文件系统有1.3G大小? 如何删减除QT5外不必要的软件包?

另外:

core-image-x11、fsl-image-gui都不是用的QT吗?

我可以bitbake core-mage-base 然后在IMAGE_INSTALL_append += " qt4" 把qt4的环境放到文件系统中吗?

标签 (2)
0 项奖励
回复
1 解答
1,509 次查看
karangajjar
Senior Contributor II

Hi luo yaojun,

You can find the packages that will be installed for an image by using below commands:

bitbake -g <image>

So, you can filter out the packages you do not want to install and remove them using PACKAGE_EXCLUDE command as in the link Yocto Project Reference Manual .

Also, you can follow Useful bitbake commands  for other useful bitbake commands.

Or

You can follow the below document to include qt in your image:

Building Qt5 using yocto on Wandboard - Wandboard Wiki 

Regards,

Karan Gajjar

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,510 次查看
karangajjar
Senior Contributor II

Hi luo yaojun,

You can find the packages that will be installed for an image by using below commands:

bitbake -g <image>

So, you can filter out the packages you do not want to install and remove them using PACKAGE_EXCLUDE command as in the link Yocto Project Reference Manual .

Also, you can follow Useful bitbake commands  for other useful bitbake commands.

Or

You can follow the below document to include qt in your image:

Building Qt5 using yocto on Wandboard - Wandboard Wiki 

Regards,

Karan Gajjar

0 项奖励
回复