Dear all,
I want to put the GPIO1_IO09 pin configured to adc function,I have modified the imx6ul-14x14-evk.dts and imx6ul.dtsi .
The following: (Red font is I modified in the imx6ul-14x14-evk.dts)
reg_sd1_vmmc: regulator@1 {
compatible = "regulator-fixed";
regulator-name = "VSD_3V3";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
//gpio = <&gpio1 9 GPIO_ACTIVE_HIGH>;
//enable-active-high;
};
reg_vref_3v3: regulator@2 {
compatible = "regulator-fixed";
regulator-name = "vref-3v3";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
};
&adc1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_adc1>;
vref-supply = <®_vref_3v3>;
status = "okay";
};
pinctrl_hog_1: hoggrp-1 {
fsl,pins = <
MX6UL_PAD_LCD_RESET__WDOG1_WDOG_ANY 0x30b0
MX6UL_PAD_UART1_RTS_B__GPIO1_IO19 0x17059 /* SD1 CD */
MX6UL_PAD_GPIO1_IO05__USDHC1_VSELECT 0x17059 /* SD1 VSELECT */
//MX6UL_PAD_GPIO1_IO09__GPIO1_IO09 0x17059 /* SD1 RESET */
>;
};
pinctrl_adc1: adc1grp {
fsl,pins = <
MX6UL_PAD_GPIO1_IO09__GPIO1_IO09 0xb0
>;
};
imx6ul.dtsi file i modified :
adc1: adc@02198000 {
compatible = "fsl,imx6ul-adc", "fsl,vf610-adc";
reg = <0x02198000 0x4000>;
interrupts = <GIC_SPI 100 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6UL_CLK_ADC1>;
num-channels = <10>;
clock-names = "adc";
status = "disabled";
When I send this pin is connected to the different voltage(3.3V or 2.5V), found the adc values will not change,
root@imx_mfgtools_nogpu:/sys/bus/iio/devices/iio:device0# cat in_voltage9_raw
4080
root@imx_mfgtools_nogpu:/sys/bus/iio/devices/iio:device0# cat in_voltage9_raw
4077
root@imx_mfgtools_nogpu:/sys/bus/iio/devices/iio:device0# cat in_voltage9_raw
Can you tell me how to modify to get the right result?
Best Regards,
xiaohuige
已解决! 转到解答。
Hi 小辉哥
this signal is used in uboot also, please try to set it as input with pull disabled,
iomux_v3_cfg_t const usdhc1_pads[]
uboot-imx.git - Freescale i.MX u-boot Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Good morning,
I am trying as well to set up the ADC on iMX6UL on my custom board.
I would like to run ADC on the following pins:
GPIO1_IO02 to GPIO1_IO07.
GPIO1_IO00 to GPIO1_IO01 I want to use as I2C pins.
GPIO1_IO08 to GPIO1_IO09 I want to use as output pins.
I understand that I need to modify in imx6ul.dtsi as follow:
num-channels = <6>;
But how to apply the offset to not start from channel 0 but 2?
Best Regards,
Krzysztof
Good morning,
I am trying to do the same with my custom board, only with the diference that I will use 10 gpios.
Using your example, i configure GPIO6 not GPIO9 like this example and I am reading ok a temperature sensor.
pinctrl_adc1: adc1grp {
fsl,pins = <
MX6UL_PAD_GPIO1_IO06__GPIO1_IO06 0xb0
>;
};
But, i need to configure other 9gpios, started form GPIO1_IO1 to GPIO1_IO9 all ADC. What I don´t know is how I must configure on the device tree, all this gpios. Maybe:
pinctrl_adc1: adc1grp {
fsl,pins = <
MX6UL_PAD_GPIO1_IO00__GPIO1_IO00 0xb0
MX6UL_PAD_GPIO1_IO01__GPIO1_IO01 0xb0
MX6UL_PAD_GPIO1_IO02__GPIO1_IO02 0xb0
MX6UL_PAD_GPIO1_IO03__GPIO1_IO03 0xb0
MX6UL_PAD_GPIO1_IO04__GPIO1_IO04 0xb0
MX6UL_PAD_GPIO1_IO05__GPIO1_IO05 0xb0
MX6UL_PAD_GPIO1_IO06__GPIO1_IO06 0xb0
MX6UL_PAD_GPIO1_IO07__GPIO1_IO07 0xb0
MX6UL_PAD_GPIO1_IO08__GPIO1_IO08 0xb0
MX6UL_PAD_GPIO1_IO09__GPIO1_IO09 0xb0
>;
};
I can´t find any information on internet. Can you help me please?
Thanks for all, best regards,
Goiatz
Hi 小辉哥
this signal is used in uboot also, please try to set it as input with pull disabled,
iomux_v3_cfg_t const usdhc1_pads[]
uboot-imx.git - Freescale i.MX u-boot Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------