imx6ul Dual ethernet connector question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6ul Dual ethernet connector question

1,058件の閲覧回数
zhangbin_eos
Contributor III

hi

board is imx6ul-14x14-evk.

Does the board's dual ethernet support independent work?
Is it possible to choose one of the ethernets to work independently, or two ethernets to work at the same time?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

917件の閲覧回数
rakesh_patel
Senior Contributor I

Hi zhangbin.eos@foxmail.com,

Yes, it is possible to use the dual ethernet port independently as well as both the ethernets at the same time.

To use only a single Ethernet, we can change the device tree node and disable the ethernet which you don't want to use.

Regards,

Rakesh

0 件の賞賛
返信

917件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which BSP is running on your board?

0 件の賞賛
返信