imx6ul 串口非标准波特率

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul 串口非标准波特率

1,960 Views
小辉哥
Contributor III

各位大佬,imx6ul,串口如何支持1000这种非标准波特率,有支持吗?该如何处理?

Labels (2)
0 Kudos
Reply
1 Reply

1,686 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

We have no ready-made non-standard baud rate scheme. However, according to the description in the chapter UART in the reference manual, the baud rate depends on the module clock, and the module clock comes from UART_CLK_ROOT. At the same time, the maximum UART_CLK_ROOT clock does not exceed 80MHz, and the default value is 4MHz. The relationship between module clock and band rate is that module clock is greater than or equal to band rate X 16.

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

According to above description, non-standard band rate should be no problem.


So you can try.

<没有现成的方案,您只能根据上面的描述,代码里去调试一下>

Have a nice day!

NXP TIC Weidong Sun