imx6sx u-boot bootaux not present in custom build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6sx u-boot bootaux not present in custom build

Jump to solution
3,369 Views
mpilia
Contributor III

Hi,

I was trying to load and run a hello_world example from FreeRTOS_BSP_1.0.1_iMX6SX/examples/imx6sx_sdb_m4/demo_apps/hello_world/armgcc (built with ./build_debug.sh) into Cortex M4 by putting the .bin file in the fat partition of the SD card, then booting the board from SD Card and stopping the u-boot before loading the kernel and giving these commands:

 

setenv m4image hello_world.bin
setenv m4runaddr 0x7f8000
setenv loadm4image 'fatload mmc ${mmcdev}:${mmcpart} ${m4runaddr} ${m4image}; dcache flush'
setenv m4boot 'run loadm4image; bootaux ${m4runaddr}'
saveenv
run m4boot

 

 

The problem is that the command bootaux is not present as you can see in the following image:

U-boot_command_no_bootaux.png

This command is  available, instead, in the U-boot in the original SD Card provided with the SABRE iMX6sx:

U-boot_original_SD_commands.png

How can I make this command available in my custom build too?

We built our custom core-image-minimal starting from https://github.com/Freescale/fsl-community-bsp-platform -b dunfell repository.

This is how our U-boot looks like:

U-boot_build_custom.png

and this is the one in the Original SD Card:

U-boot_Original_SD_Card.png

By the way, I tried to accomplish the same task using the Original SD Card

Run_M4_fw.png

but no output is coming out from the M4 uart. Have I to modify anything? Do you confirm that I have not to modify the .dtb files related to the kernel?

Thanks in advance.

 

0 Kudos
Reply
1 Solution
3,299 Views
mpilia
Contributor III

Hi,

I get the solution from this post. In this way there is no need to modify M4 uart clock rate in the dbg_uart_init.

View solution in original post

5 Replies
3,361 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Please try by adding the following to your defconfig:

CONFIG_IMX_BOOTAUX=y


As for the M4-UART not displaying anything it may not be loaded correctly, could you try with the following:

Load the application image from the SD card to DDR RAM:
fatload mmc 2:1 0x7F8000 <M4_example>.bin

Flush cached content to DDR RAM:
dcache flush
Copy Cortex-M4 image from DDR RAM to TCM:
cp.b 0x80000000 0x7F8000 0x8000
Flush cached content to TCM:
dcache flush
Start the Cortex-M4 core from the TCM:
bootaux 0x7F8000

Best regards,
Aldo.

0 Kudos
Reply
3,330 Views
mpilia
Contributor III

Hi,

thank you very much for the advises. I tried to add intermediate copy to DDR memory before the TCM one and it works fine. I did it with the bootloader provided with original SD Card.

I'm not sure instead which defconfig file I have to modify in order to add the "CONFIG_IMX_BOOTAUX=y". I found different ones in the folder /sources/meta-freescale/recipes-kernel/linux/[...] but I do not know which is the one.

 

Thank you again

Massimo

0 Kudos
Reply
3,306 Views
mpilia
Contributor III

Hi Aldo and thank you for your reply, I will check the links you suggested for doing configuration changes.

At the same time I was trying the freertos pingpong example provided in the FreeRTOS_BSP_1.0.1_iMX6SX/examples/imx6sx_sdb_m4/demo_apps/rpmsg/pingpong_freertos. After compiling and copying the rpmsg_pingpong_freertos_example.bin to the SD Card I Switch on the board and stop normal booting. After that I run the rpmsg_pingpong_freertos_example.bin and in the M4 core serial interface i see this output

 

 

RPMSG PingPong FreeRTOS API Demo...
RPMSG Init as Remote

 

 

 

After that I boot the A9, log in and give the command: 

insmod /lib/modules/4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d/kernel/drivers/rpmsg/imx_rpmsg_pingpong.ko

On the A9 side I see this:

Schermata da 2021-02-10 15-01-07.png

and on the M4 side this:

Schermata da 2021-02-10 14-46-10.png

Seeing the contents of the PingPongTask in the pingpong_freertos.c file

 

 

static void PingPongTask (void* param)
{
    int result;
    struct remote_device *rdev = NULL;
    struct rpmsg_channel *app_chnl = NULL;
    THE_MESSAGE msg = {0};
    int len;

    /* Print the initial banner */
    PRINTF("\r\nRPMSG PingPong FreeRTOS RTOS API Demo...\r\n");

    PRINTF("RPMSG Init as Remote\r\n");
    result = rpmsg_rtos_init(0 /*REMOTE_CPU_ID*/, &rdev, RPMSG_MASTER, &app_chnl);
    assert(0 == result);

    PRINTF("Name service handshake is done, M4 has setup a rpmsg channel [%d ---> %d]\r\n", app_chnl->src, app_chnl->dst);

    while (true)
    {
        /* receive/send data to channel default ept */
        result = rpmsg_rtos_recv(app_chnl->rp_ept, &msg, &len, sizeof(THE_MESSAGE), NULL, 0xFFFFFFFF);
        assert(0 == result);
        PRINTF("Get Data From Master Side : %d\r\n", msg.DATA);
        msg.DATA++;
        result = rpmsg_rtos_send(app_chnl->rp_ept, &msg, sizeof(THE_MESSAGE), app_chnl->dst);
        assert(0 == result);
    }

    /* If destruction required */
    /*
    PRINTF("\r\nMessage pingpong finished\r\n");

    rpmsg_rtos_deinit(rdev);
    */
}

 

 

On the M4 side I expected to see the string "Name service handshake is done, M4 has setup a rpmsg channel [src ---> dst]" and then some strings "Get Data From Master Side: data", like this:

M4 has setup a rpmsg channel [---> 1]
Get Data From Master Side: 1
Get Data From Master Side: 3
Get Data From Master Side: 5
Get Data From Master Side: 7
...

but I only see a succession of incomprehensible characters. 

Despite this, on the A9 side it would still seem that the data is correctly increased.

 

If then I modify the clock rate of the M4 uart from 24MHz to 80MHz in the dbg_uart_init function in board.c file,

// DbgConsole_Init(BOARD_DEBUG_UART_BASEADDR, 24000000, 115200);
DbgConsole_Init(BOARD_DEBUG_UART_BASEADDR, 80000000, 115200);

I can see the correct string coming with the data from A9, but the first ones, just at the startup of the M4, are unreadable

Schermata da 2021-02-10 16-24-51.png

How to fix this?

 

0 Kudos
Reply
3,300 Views
mpilia
Contributor III

Hi,

I get the solution from this post. In this way there is no need to modify M4 uart clock rate in the dbg_uart_init.