imx6sx remoteproc?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6sx remoteproc?

1,144 Views
davidpatton
Contributor III

Has anyone ever used this? Loading from u-boot seems fine during development, but as a final product, remoteproc is much more attractive, I can load the M4 after linux is up, and if the M4 trips, I can restart it, without having to reboot the entire board. There seems to be little, if any, information on remoteproc outside of the OMAP world.Thanks...

Labels (3)
Tags (2)
0 Kudos
3 Replies

916 Views
terry_lv
NXP Employee
NXP Employee

Hi,

  Currently, iMX6SX and iMX7D don't support remoteproc.

  Remoteproc need a resource table in M4 image. As iMX6SX and iMX7D SDK don't have new releases, resource table will not be added to their SDK.

  Thanks!

Regards

Terry

0 Kudos

919 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 Kudos

919 Views
davidpatton
Contributor III

Thanks for the reply. The first link only mentions MCC then later on mention that RPMsg will be supported. The second link uses u-boot to load the second core. The third link mentions remoteproc but never actually describes how to set it up or use it.

0 Kudos