Hello Everybody,
I have a bare-metal code running on M4 core.
The core executes, from DDR, much slower than expected, that means more than 10 times slower than executing from TCM.
I suspect the cache is not properly configured.
The cache controller is enabled using the LMEM_EnableSystemCache() and LMEM_EnableCodeCache() provided by NXP on FreeRTOS example.There is no effect for execution time after calling LMEM functions.
I did not find anything about cacheability.
Is there any way to define/check the DDR cacheability for M4? I mean to define DDR regions as cacheable/non-cacheable.
Thanks
解決済! 解決策の投稿を見る。
Hello,
The base address of LMEM is 0xE008_2000.
The RM in section 13.11 (LMEM Memory Map/Register Definition) contains
misprints.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
The base address of LMEM is 0xE008_2000.
The RM in section 13.11 (LMEM Memory Map/Register Definition) contains
misprints.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Yuri,
I have updated the base address. The cache is working now, the execution time is as expected.
After enabling the cache, the Segger J-Link debugger seems not able to stop in breakpoints. Do you have any hint for that?
Regards,
Catalin
Hi, as I understood the cacheability has effect on the whole DDR region, right? Is it possible to enable the cacheability for a specified DDR region?
Hello,
perhaps the problem concerns with the fact, that cache coherency
is not provided in i.MX6 SX. The debugger is working in physical addresses.
Regards,
Yuri.
Thanks Yuri