I want to add two Volume addition and subtraction buttons,should i add this two GPIO to 1.8V CSI module which control WM8962BECSN/R or other Casual 3.3V module?
Hi zhang
for volume control examples one can check sect.28.5.1 Stereo Codec Unit Test
attached Linux Manual and unit test package ( ../mxc_sound_test)
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
You misunderstood what I meant. I didn't want to ask you about the software. What I want to ask is about the hardware ,where do I connect the Volume adjustment button. Is 1.8V gpio or the 3.3V GPIO?
you can use any gpio for such purpose, ir does not not matter "1.8V gpio or the 3.3V GPIO".
ok ,thanks very much!