imx6solo yocto-4.14.78 imx-gpu-sdk fails to compile

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6solo yocto-4.14.78 imx-gpu-sdk fails to compile

Jump to solution
1,849 Views
liqun_wei
Contributor III

imx6solo yocto-4.14.78 imx-gpu-sdk fails to compile

Package location: /work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/git/DemoFramework/FslBase

Package build arguments1: ['install']
General build arguments2: ['install']
Running Yocto checks
- Common SDK environment
Configuration check completed successfully.
arm-poky-linux-gnueabi-g++ -march=armv7-a -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a9 --sysroot=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot -DNDEBUG -O2 -pipe -g -feliminate-unused-debug-types -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0=/usr/src/debug/imx-gpu-sdk/5.2.0-r0 -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot= -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot-native= -fvisibility-inlines-hidden -O3 -Wall -Wtype-limits -Wuninitialized -fPIC -DPIC -std=c++11 -g -DFSL_FEATURE_STB -DFSL_FEATURE_FSLBASE -pthread -DFSL_PLATFORM_YOCTO -fno-strict-aliasing -fno-optimize-sibling-calls -DLINUX -I/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot/usr/include -I/inc -Iinclude -I/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/git/.Thirdparty/Yocto/Make/tclap-1.2.2/include -o build/Yocto/obj/Release/source/FslBase/Bits/ByteArrayUtil.o -c source/FslBase/Bits/ByteArrayUtil.cpp
make: arm-poky-linux-gnueabi-g++: Command not found
arm-poky-linux-gnueabi-g++ -march=armv7-a -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a9 --sysroot=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot -DNDEBUG -O2 -pipe -g -feliminate-unused-debug-types -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0=/usr/src/debug/imx-gpu-sdk/5.2.0-r0 -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot= -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot-native= -fvisibility-inlines-hidden -O3 -Wall -Wtype-limits -Wuninitialized -fPIC -DPIC -std=c++11 -g -DFSL_FEATURE_STB -DFSL_FEATURE_FSLBASE -pthread -DFSL_PLATFORM_YOCTO -fno-strict-aliasing -fno-optimize-sibling-calls -DLINUX -I/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot/usr/include -I/inc -Iinclude -I/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/git/.Thirdparty/Yocto/Make/tclap-1.2.2/include -o build/Yocto/obj/Release/source/FslBase/Compression/ValueCompression.o -c source/FslBase/Compression/ValueCompression.cpp
make: arm-poky-linux-gnueabi-g++: Command not found
make: *** [build/Yocto/obj/Release/source/FslBase/Bits/ByteArrayUtil.o] Error 127
make: *** Waiting for unfinished jobs....
make: *** [build/Yocto/obj/Release/source/FslBase/Compression/ValueCompression.o] Error 127
arm-poky-linux-gnueabi-g++ -march=armv7-a -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a9 --sysroot=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot -DNDEBUG -O2 -pipe -g -feliminate-unused-debug-types -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0=/usr/src/debug/imx-gpu-sdk/5.2.0-r0 -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot= -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot-native= -fvisibility-inlines-hidden -O3 -Wall -Wtype-limits -Wuninitialized -fPIC -DPIC -std=c++11 -g -DFSL_FEATURE_STB -DFSL_FEATURE_FSLBASE -pthread -DFSL_PLATFORM_YOCTO -fno-strict-aliasing -fno-optimize-sibling-calls -DLINUX -I/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot/usr/include -I/inc -Iinclude -I/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/git/.Thirdparty/Yocto/Make/tclap-1.2.2/include -o build/Yocto/obj/Release/source/FslBase/Getopt/Option.o -c source/FslBase/Getopt/Option.cpp
make: arm-poky-linux-gnueabi-g++: Command not found
make: *** [build/Yocto/obj/Release/source/FslBase/Getopt/Option.o] Error 127

Labels (3)
Tags (3)
0 Kudos
1 Solution
1,465 Views
liqun_wei
Contributor III

Okay, I've compiled successfully.

The problem is that my project failed to download some packages.

Thank you.

View solution in original post

0 Kudos
3 Replies
1,465 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Liqun,

There should be some problems with the toolchain arm-poky-linux-gnueabi-g++: Command not found, try to fix this or installing all yocto packages.

Regards

0 Kudos
1,466 Views
liqun_wei
Contributor III

Okay, I've compiled successfully.

The problem is that my project failed to download some packages.

Thank you.

0 Kudos
1,465 Views
liqun_wei
Contributor III

But, I have compiled successfully with the following commands:

DISTRO=fsl-imx-fb MACHINE=imx6solosabresd source fsl-setup-release.sh -b build_qt5

bitbake fsl-image-qt5-validation-imx

bitbake meta-toolchain-qt5 -c populate_sdk

and with the same yocto project, I failed with these commands:

DISTRO=fsl-imx-wayland MACHINE=imx6solosabresd source fsl-setup-release.sh -b build_wayland

bitbake fsl-image-qt5-validation-imx

bitbake meta-toolchain-qt5 -c populate_sdk

How could be this result?

thanks for your reply.

0 Kudos