imx6solo yocto-4.14.78 imx-gpu-sdk fails to compile
Package location: /work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/git/DemoFramework/FslBase
Package build arguments1: ['install']
General build arguments2: ['install']
Running Yocto checks
- Common SDK environment
Configuration check completed successfully.
arm-poky-linux-gnueabi-g++ -march=armv7-a -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a9 --sysroot=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot -DNDEBUG -O2 -pipe -g -feliminate-unused-debug-types -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0=/usr/src/debug/imx-gpu-sdk/5.2.0-r0 -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot= -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot-native= -fvisibility-inlines-hidden -O3 -Wall -Wtype-limits -Wuninitialized -fPIC -DPIC -std=c++11 -g -DFSL_FEATURE_STB -DFSL_FEATURE_FSLBASE -pthread -DFSL_PLATFORM_YOCTO -fno-strict-aliasing -fno-optimize-sibling-calls -DLINUX -I/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot/usr/include -I/inc -Iinclude -I/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/git/.Thirdparty/Yocto/Make/tclap-1.2.2/include -o build/Yocto/obj/Release/source/FslBase/Bits/ByteArrayUtil.o -c source/FslBase/Bits/ByteArrayUtil.cpp
make: arm-poky-linux-gnueabi-g++: Command not found
arm-poky-linux-gnueabi-g++ -march=armv7-a -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a9 --sysroot=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot -DNDEBUG -O2 -pipe -g -feliminate-unused-debug-types -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0=/usr/src/debug/imx-gpu-sdk/5.2.0-r0 -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot= -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot-native= -fvisibility-inlines-hidden -O3 -Wall -Wtype-limits -Wuninitialized -fPIC -DPIC -std=c++11 -g -DFSL_FEATURE_STB -DFSL_FEATURE_FSLBASE -pthread -DFSL_PLATFORM_YOCTO -fno-strict-aliasing -fno-optimize-sibling-calls -DLINUX -I/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot/usr/include -I/inc -Iinclude -I/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/git/.Thirdparty/Yocto/Make/tclap-1.2.2/include -o build/Yocto/obj/Release/source/FslBase/Compression/ValueCompression.o -c source/FslBase/Compression/ValueCompression.cpp
make: arm-poky-linux-gnueabi-g++: Command not found
make: *** [build/Yocto/obj/Release/source/FslBase/Bits/ByteArrayUtil.o] Error 127
make: *** Waiting for unfinished jobs....
make: *** [build/Yocto/obj/Release/source/FslBase/Compression/ValueCompression.o] Error 127
arm-poky-linux-gnueabi-g++ -march=armv7-a -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a9 --sysroot=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot -DNDEBUG -O2 -pipe -g -feliminate-unused-debug-types -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0=/usr/src/debug/imx-gpu-sdk/5.2.0-r0 -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot= -fdebug-prefix-map=/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot-native= -fvisibility-inlines-hidden -O3 -Wall -Wtype-limits -Wuninitialized -fPIC -DPIC -std=c++11 -g -DFSL_FEATURE_STB -DFSL_FEATURE_FSLBASE -pthread -DFSL_PLATFORM_YOCTO -fno-strict-aliasing -fno-optimize-sibling-calls -DLINUX -I/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/recipe-sysroot/usr/include -I/inc -Iinclude -I/work/imx-yocto-bsp/build_wayland/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-sdk/5.2.0-r0/git/.Thirdparty/Yocto/Make/tclap-1.2.2/include -o build/Yocto/obj/Release/source/FslBase/Getopt/Option.o -c source/FslBase/Getopt/Option.cpp
make: arm-poky-linux-gnueabi-g++: Command not found
make: *** [build/Yocto/obj/Release/source/FslBase/Getopt/Option.o] Error 127
Solved! Go to Solution.
Okay, I've compiled successfully.
The problem is that my project failed to download some packages.
Thank you.
Hello Liqun,
There should be some problems with the toolchain arm-poky-linux-gnueabi-g++: Command not found, try to fix this or installing all yocto packages.
Regards
Okay, I've compiled successfully.
The problem is that my project failed to download some packages.
Thank you.
But, I have compiled successfully with the following commands:
DISTRO=fsl-imx-fb MACHINE=imx6solosabresd source fsl-setup-release.sh -b build_qt5
bitbake fsl-image-qt5-validation-imx
bitbake meta-toolchain-qt5 -c populate_sdk
and with the same yocto project, I failed with these commands:
DISTRO=fsl-imx-wayland MACHINE=imx6solosabresd source fsl-setup-release.sh -b build_wayland
bitbake fsl-image-qt5-validation-imx
bitbake meta-toolchain-qt5 -c populate_sdk
How could be this result?
thanks for your reply.