imx6solo文件系统带QT5.6.1 webengine

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6solo文件系统带QT5.6.1 webengine

2,477 Views
1182614726
Contributor III

大家好,

            目前使用imx6solo芯片,yocto BSP版本为L4.1.15-2.1.0,目前使用bitbake fsl-image-qt5,编译QT版本。

            发现编译生成的QT版本为5.6.1,文件系统带QT,但是文件系统中的QT5.6.1不带webengine,请问要如何编译,QT5.6.1中带webengine。

      

            谢谢

Labels (1)
0 Kudos
10 Replies

2,241 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the chapter 5.6.7 Qt 5 and QtWebEngine browsers of 4.1.15 i.MX Yocto Project User's Guide

0 Kudos

2,241 Views
1182614726
Contributor III

你好 Joan,

                 你好像并没有理解我的意思,谢谢。

                 我查看了你说的这个地方,描述的内容与我所提的问题不相干,谢谢

0 Kudos

2,241 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the yocto user guide:

There are three Qt 5 browsers available. QtWebEngine browsers can be found in /usr/share/qt5/examples/
webenginewidgets/browser, /usr/share/qt5/examples/webenginewidgets/fancybrowser and /usr/
share/qt5/examples/webengine/quicknanobrowser.

after you built the qt, you couldn't find the qtwebengine browsers as mentioned path?

0 Kudos

2,241 Views
1182614726
Contributor III

Hi Joan,

               I didn't found anything about webengine in the directory you said.

               Thank you very much

0 Kudos

2,241 Views
joanxie
NXP TechSupport
NXP TechSupport

what backend do you use? suggest to use DISTRO=fsl-imx-wayland,

0 Kudos

2,241 Views
1182614726
Contributor III

Hi Joan,

            我目前使用的backend为framebuffer,为什么建议使用wayland呢?

            使用framebuffer有什么bug吗?

            谢谢

0 Kudos

2,241 Views
joanxie
NXP TechSupport
NXP TechSupport

sorry for the confused answer, let me double check it, because this is very old bsp, I haven't built it on my board, I need to check this

0 Kudos

2,241 Views
1182614726
Contributor III

Hi Joan,

            我们选用imx6solo芯片的时候,你们代理推荐我们购买imx6dl的开发板,并建议使用L4.1.15-2.1.0的BSP。

            还望帮忙确认,谢谢

0 Kudos

2,241 Views
joanxie
NXP TechSupport
NXP TechSupport

I checked that we built qt on all backend of4.1.15, but not built qtwebengine on fb backend, only xwayland, so couldn't say if qtwebengine works on fb backend, since you built fb, don't have qtwebengine, pls try to built xwayland, we have tested on that.

2,241 Views
1182614726
Contributor III

Hi Joan,

            非常感谢你的回答,谢谢。

0 Kudos