imx6sllevk fails to flash rootfs.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6sllevk fails to flash rootfs.

1,034 Views
sujay1
Contributor V

I added a thread here https://community.nxp.com/thread/516958  but there seems to be no valid solution.

can someone please suggest something?

or maybe post the u-boot binary so that I can bring up the board?

0 Kudos
Reply
1 Reply

954 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sujay

actually in that thread you used custom imx6sll board with 512 MB LPDDR2 DRAM,

not nxp imx6sllevk reference board which used lpddr3 memory. So nxp imx6sllevk reference

demo images did not run. NXP has special service for helping customers with software customizations:

Commercial Support and Engineering Services | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply