imx6sllevk fails to flash rootfs.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6sllevk fails to flash rootfs.

632件の閲覧回数
sujay1
Contributor V

I added a thread here https://community.nxp.com/thread/516958  but there seems to be no valid solution.

can someone please suggest something?

or maybe post the u-boot binary so that I can bring up the board?

0 件の賞賛
返信
1 返信

552件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sujay

actually in that thread you used custom imx6sll board with 512 MB LPDDR2 DRAM,

not nxp imx6sllevk reference board which used lpddr3 memory. So nxp imx6sllevk reference

demo images did not run. NXP has special service for helping customers with software customizations:

Commercial Support and Engineering Services | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信