imx6sl uboot shutdown

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6sl uboot shutdown

591 Views
yan2anfei
Contributor III

hi ,

   I have a imx6slevk board, I want't shutdown my system in uboot.

   I set the register SNVS_LPCR's TOP and DP_EN bit . 

   The system didn't power off but reboot.

   Is something else need set ?

thanks!

Labels (2)
0 Kudos
2 Replies

440 Views
igorpadykov
NXP Employee
NXP Employee

Hi yan2

please check that pmic licell is attached, so there is permanent

vsnvs voltage applied to processor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

440 Views
yan2anfei
Contributor III

hi igorpadykov,

  Thanks for your reply !

  If add licell, the linux system halt function is ok. but the uboot power off  is reboot still.

 the VDD_SNVS_IN PIN is 3v didn't pull down.

 thanks!

0 Kudos