hi ,
my chip is imx6sl, I use uart4 with rts and cts ,
the set is as follow. but the imx6sl's rts pin (MX6SL_PAD_SD1_DAT6__UART4_RTS_B) is always high.
whether should I pull it down force or my set is something wrong.
pinctrl_uart4_1: uart4grp-1 {
fsl,pins = <
MX6SL_PAD_SD1_DAT4__UART4_RX_DATA 0x1b0b1
MX6SL_PAD_SD1_DAT5__UART4_TX_DATA 0x1b0b1
MX6SL_PAD_SD1_DAT7__UART4_CTS_B 0x1b0b1
MX6SL_PAD_SD1_DAT6__UART4_RTS_B 0x1b0b1
>;
};
&uart4 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart4_1>;
fsl,uart-has-rtscts;
status = "okay";
/* for DTE mode, add below change */
/* fsl,dte-mode; */
/* pinctrl-0 = <&pinctrl_uart4dte_1>; */
};
&usdhc1 {
status = "disabled";
};
解決済! 解決策の投稿を見る。
Hi yan2
UART_RTS direction is output in DTE mode according to
Table 55. UART I/O Configuration vs. Mode i.MX6SL Datasheet
https://www.nxp.com/docs/en/data-sheet/IMX6SLCEC.pdf
so one can try to uncomment dte statement in dts file and check
bit DCEDTE in UARTx_UFCR register.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi yan2
UART_RTS direction is output in DTE mode according to
Table 55. UART I/O Configuration vs. Mode i.MX6SL Datasheet
https://www.nxp.com/docs/en/data-sheet/IMX6SLCEC.pdf
so one can try to uncomment dte statement in dts file and check
bit DCEDTE in UARTx_UFCR register.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thank you very much.