imx6sl powerkey wakeup system

cancel
Showing results for 
Search instead for 
Did you mean: 

imx6sl powerkey wakeup system

531 Views
yan2anfei
Contributor III

hi, 

I want to wakeup my system from sleep mode (echo mem>/sys/power/state) when press the powerkey which connect to the imx6sl  ONOFF pin.

but it failed.  the chip of imx7d  can achieve this function.

Is imx6sl's ONOFF key didn't has the function wakeup system.   

my software environment: yocto L4.1.15_2.1.0-ga.

hardware envionment mcimx6slevk

modify the imx6sl.dtsi as follow:

snvs: snvs@020cc000 {
compatible = "fsl,sec-v4.0-mon", "syscon", "simple-mfd";
reg = <0x020cc000 0x4000>;

snvs_rtc: snvs-rtc-lp {
compatible = "fsl,sec-v4.0-mon-rtc-lp";
regmap = <&snvs>;
offset = <0x34>;
interrupts = <0 19 IRQ_TYPE_LEVEL_HIGH>,
<0 20 IRQ_TYPE_LEVEL_HIGH>;
};

snvs_pwrkey: snvs-powerkey {
compatible = "fsl,sec-v4.0-pwrkey";
regmap = <&snvs>;
interrupts = <0 4 IRQ_TYPE_LEVEL_HIGH>;
linux,keycode = <116>;
gpio-key,wakeup;
};

snvs_poweroff: snvs-poweroff {
compatible = "syscon-poweroff";
regmap = <&snvs>;
offset = <0x38>;
mask = <0x61>;
status = "disabled";
};
};

thandks & best regards.

Labels (2)
0 Kudos
1 Reply

237 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi yan2

what bsp used in the case, please try with nxp bsps described on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

try snvs_pwrkey example as in  imx6sx.dtsi

linux-imx.git - i.MX Linux Kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos