imx6sl crash issue when the current suddenly high

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6sl crash issue when the current suddenly high

ソリューションへジャンプ
1,463件の閲覧回数
张松源
Contributor III

  Hi,

   

   our machine do the aging test. it will crash without any kernel log. it is so hard to analyse。

   when the machine stop update display, most of  time, the supply current is keep 15mA, but it will suddenly change to 40mA, about 1 second ago, the current back to 15mA.

   

    Every time when our device crash, the supply current is 40mA. then the power button doesn't work, the console couldn't input any word. and it will happen when wifi off( if wifi on, it will not crash but power consumption very high).

     

best regard!

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,371件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 张 松源

please check power supply requirements described in

i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

and test memory with ddr test :

https://community.nxp.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,371件の閲覧回数
张松源
Contributor III

the DDR stress test is OK, I will check the "User’s Guide".

Best regards,

songyuan

0 件の賞賛
返信
1,372件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 张 松源

please check power supply requirements described in

i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

and test memory with ddr test :

https://community.nxp.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------