Hi All,
I have to make lvds display (HiMax 8282A)work in uboot and kernel. I added the initialization sequence and other code change as per spec of LVDS in uboot bt nothing seems to comming up.
1) Can somebody please point me to the reference code or documents for LVDS splash screen support and other required change for making LVDS work ?
2) other question is about Splash screen BMP file , where/how and on which partition i need to write my BMP file and reference steps?
3) any patch from freescale to support splash screen and LVDS in uboot and kernel ?
thanks
Robin Singh
已解决! 转到解答。
Working for now.
Followed this for uboot splash screen with RGB color filled.
only uboot patch L
[2015-12-21 Update]: Added 3.10.53_GA1.1.0 patch: L3.10.53_GA1.1.0_uboot_logo_keep_patch_2015-12-21.zip.
Verified on iMX6DL/Q SabreSD board. It supports LCD and LVDS panels, HDMI patch will be released later.
Kernel side only LCD init code and DTS setting change is required.
We are using imx6q customized board , the panel K&D-WXGA is detected in uboot 2017 with resolution 1280x800 works in Android but when we boots in linux , we get the following error,
"
mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
ldb 2000000.aips-bus:ldb@020e0008: failed to get clk choice0
ldb 2000000.aips-bus:ldb@020e0008: failed to get clk choice1
ldb 2000000.aips-bus:ldb@020e0008: f
ldb 2000000.aips-bus:ldb@020e0008: failed to get clk choice3
mxc_sdc_fb fb@0: registered mxc display driver ldb
mxc_sdc_fb fb@0: 1024x768 h_sync,r,l: 60,40,220 v_sync,l,u: 10,7,21
pixclock=65002000 Hz
imx-ipuv3 2800000.ipu: try ipu internal clk
imx-ipuv3 2800000.ipu: disp=1, pixel_clk=65002000 64653061 parent=64653061 div=1
"
please help us to fix the issue..
we have set 1280x800 in imx6qdl-sabresd.dtsi file of kernel 4.1.15 , and the mx6sabresd.c file of uboot version 2017, the set resolution is not taken when we boot in linux it takes the default value 1024x768 ..
how to pass / change the resolution value in linux ..
Hi robin
lvds splash screen is supported, for example check vidinfo_t panel_info:
uboot-imx.git - Freescale i.MX u-boot Tree
descriptions:
https://boundarydevices.com/displaying-a-splash-screen-with-u-boot/
uboot-imx.git - Freescale i.MX u-boot Tree
How to change SABRE-SD screen resolution in LOLLIPOP(5.0.0?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Working for now.
Followed this for uboot splash screen with RGB color filled.
only uboot patch L
[2015-12-21 Update]: Added 3.10.53_GA1.1.0 patch: L3.10.53_GA1.1.0_uboot_logo_keep_patch_2015-12-21.zip.
Verified on iMX6DL/Q SabreSD board. It supports LCD and LVDS panels, HDMI patch will be released later.
Kernel side only LCD init code and DTS setting change is required.