Hello, thank you for answering.
I replaced the SDcard just to be sure it is not the problem.
My board is MCIMX6Q-SDB SCH 27516 Rev C2
I don't understand why you say "it look like you don't have any kernel on it" because as you can see in the TXT file I attached last time the Kernel is booting
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 6.6.52-lts-next-ge0f9e2afd4cf (oe-user@oe-host) (arm-poky-linux-gnueabi-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240723) #1 SMP PREEMPT Tue Nov 19 23:01:49 UTC 2024
However this is the sequence I followed in "verbatim mode":
- I started following the NXP user guide UG10164
- mkdir yocto-mx6-scarthgap; cd yocto-mx6-scarthgap
- repo init -u https://github.com/nxp-imx/imx-manifest \
-b imx-linux-scarthgap -m imx-6.6.52-2.2.0.xml - repo sync -j8
- DISTRO=fsl-imx-wayland MACHINE=imx6qsabresd source imx-setup-release.sh -b build
- bitbake core-image-minimal
then I flashed the image on the SDCARD
core-image-minimal-imx6qsabresd.rootfs-20250804102423.wic.bmap
core-image-minimal-imx6qsabresd.rootfs-20250804102423.wic.zst
then I verified DIP Switch SW6 to boot form SDcard in slot SD3
OFF-ON-OFF-OFF-OFF-OFF-ON-OFF
Then I powered the board on: See the new file attached