I am trying to use u-boot, kernel and rootfs on the imx6qsabresd board without using yocto.
I put u-boot, kernel, and rootfs on the sd card and booted it.
-Waiting for root device /dev/mmcblk1p2...
-random: crng init done
No message appears after the message is printed.
In my opinion, u-boot and kernel are working, and rootfs seems to have a problem.
The sites I referenced are as follows.
-https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Installing-Ubuntu-Rootfs-on-NXP-i-MX6-bo...
-https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Building-Linux-Kernel/ta-p/1110576#toc-h...
Download list
-Cross compiler: gcc-arm-linux-gnueabihf (latest)
-u-boot: boundarydevices/u-boot-imx6/boundary-v2017.03
-kernel: boundarydevices/linux-imx6boundary-imx_4.14.x_2.0.0_ga
-rootfs: Installing with debootstrap(base ubuntu 18.04 LTS)
full LOG : attached
Thank you
Hi jinsoo
for boundarydevices software one can look at below tutorial :
https://boundarydevices.com/customizing-ubuntudebian-kernels/
reason for "No message" may be that software was built for boundary boards,
not for imx6qsabresd board.
Best regards
igor