imx6qp ocram和uboot问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6qp ocram和uboot问题

2,919 Views
Harris
Contributor III

大家好:

    最近在调一个imx6qp的板子(sabresd sdb),有一个疑问想跟大家请教一下。

   我看到有资料说,板子在上电后,boot rom会先拷贝IVT,Boot Data,设备配置数据DCD和用户代码数据等信息到片上ram(ocram)中,然后再根据这些信息启动uboot,那么最后uboot是运行在ocram中呢,还是运行在ddr里面的呢?是否有这方面相关的资料呢?

谢谢。

Labels (2)
0 Kudos
Reply
2 Replies

1,222 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Harris,

    After power up, ROM CODE in CPU will read 4K code from Flash/SD card/eMMC to internal RAM, in the 4K data, code for DDR initialization is included, and will be used to initialize DDR, after DDR initialization is done, full u-boot will be loaded into DDR.

   So finally u-boot will run in DDR

   More information can be found in chapter boot flow in reference manual.

Have a nice day!

NXP TIC weidong sun

1,222 Views
Harris
Contributor III

Thank you very much!

0 Kudos
Reply