imx6q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q

2,832 次查看
一个人的城市
Contributor I

Hello!I created image,and the kernel version is 4.1.15.I use this command:DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11 and bitbake fsl-image-qt5;but after starting,i want to show my own desktop,For example, a simple QT program,what should i do?I am a novice ,I hope you can give me some advices.Thanks

标签 (2)
0 项奖励
回复
2 回复数

1,947 次查看
b36401
NXP Employee
NXP Employee

You need to add your application to startup for it ru run automatically when the OS starts up.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,947 次查看
一个人的城市
Contributor I

Where to add? And where is the desktop system started?Can you tell me in detail!Thanks

0 项奖励
回复