Hi All,
i am using the imx6qdl linux-imx krogoth yocto source version (imx-4.1-krogoth -m imx-4.1.15-2.1.0) ,
i am having single main thread where i am using the xcopyarea, xlib function, i am seeing the xwayland process memory is increasing, later the unit is freeze
To rootcause analaysis this ,
1. commenting the xcopyarea(), all looks fine
2. i tried enabling expose event and handle it before xcopyarea still increasing
3 . i tried enabling expose event and handle it after xcopyarea still increasing
4. i am using
PREFERRED_VERSION_gcc = "4.9%"
DISTRO_FEATURES_remove = "directfb"
DISTRO_FEATURES_append = "x11 wayland pam opengl "
SOC_FAMILY = "mx6:mx6q:mx6dl"
Note:
i am getting only noexpose events if i enable Graphicsexpose,
in blogs i am seeing lot of issue regards this but none help..
if anyone face this please provide you thoughts or input.
i tried this applingg which mentions that leak solve, v2-05-14-imx-gpu-viv-Upgrade-to-6.2.2.p0.patch but i end up in getting error .