imx6q xwayland process weston-wayland memory eating

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q xwayland process weston-wayland memory eating

2,009件の閲覧回数
shashikanthirem
Contributor III

Hi All,

i am using the imx6qdl linux-imx krogoth yocto source version (imx-4.1-krogoth -m imx-4.1.15-2.1.0) ,

i am having single main thread where i am using the xcopyarea, xlib function, i am seeing the xwayland process memory is increasing, later the unit is freeze

To rootcause  analaysis this ,

1. commenting the xcopyarea(), all looks fine

2. i tried enabling expose event and handle it before xcopyarea  still increasing 

3 .  i tried enabling expose event and handle it after xcopyarea still increasing 

4. i am using 

PREFERRED_VERSION_gcc = "4.9%"

DISTRO_FEATURES_remove = "directfb"
DISTRO_FEATURES_append = "x11 wayland pam opengl "

SOC_FAMILY = "mx6:mx6q:mx6dl"

Note:

i am getting only noexpose events if i enable Graphicsexpose, 

in blogs i am seeing lot of issue regards this but none help..

if anyone face this please provide you thoughts or input.

i tried this applingg which mentions that leak solve, v2-05-14-imx-gpu-viv-Upgrade-to-6.2.2.p0.patch but i end up in getting error .

ラベル(2)
0 件の賞賛
返信
4 返答(返信)

1,838件の閲覧回数
shashikanthirem
Contributor III

if any related patch it would be helpful

i am using 

weston 1.9

xlib 1.6.3

any recipe information required let me know

0 件の賞賛
返信

1,838件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello shashikant,

You might try the latest BSP since a lot of bug like this are fixed:

i.MX Software | NXP 

Regards

0 件の賞賛
返信

1,838件の閲覧回数
shashikanthirem
Contributor III

Hi

migration of BSP is bit difficult this time, as we have create a patch, where our OS  and application is running successfully,

so need to figure how xcopyarea is creating issue 

0 件の賞賛
返信

1,838件の閲覧回数
shashikanthirem
Contributor III

Any suggestions???

0 件の賞賛
返信