hi :
i use a imx6q board and kernel linux3.0.35,We want to turn it into a real-time system with xenomai。But when we put a patch into the kernel, we always get Incorrect results。we use linux3.0.35 and xenomai-2.6.4。 The version of patch is adeos-ipipe-3.0.43-mx6q-1.18-14.patch。
The log message is prepare-kernel.sh: Unable to patch kernel 3.0.35 with adeos-ipipe-3.0.43-mx6q-1.18-14.patch.
which version of patch should i use?? some one help me??
maybe kernel version not match ipipe patch version
Hi,
unfortunately xenomai is not supported in nxp linux bsps, this may be
posted this on meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
You can see the thread Adeneo Embedded - a whitepaper on integrating Xenomai on i.MX6 Linux
Real-time Linux with Xenomai on Freescale i.MX6
Hope this can do help for you
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Real-time Linux with Xenomai on Freescale i.MX6 This link won't open.